POSTED BY:
Bill
,
plano, tx
Overall rating:
4.0 out of 5
"the only thing that keeps this from being a 5 star rating is the location of the recharge port"
POSTED BY:
Enterprisehunter
,
MIami, Fla.
Overall rating:
5.0 out of 5
"I love this thing. This gadget will changes the way of computing. Everything a PC can do in a fantastic package. Ended up buying 2."
POSTED BY:
Wdinidaho
,
Mountain Home, ID
Overall rating:
5.0 out of 5
"The Excite Tablet is easy to use, fun and very efficient! I am impressed with the speed and performance of the Excite. I had a iPad 3 and although there are a few differences...the Excite still pleases me! Thanks Toshiba!"
POSTED BY:
sdflipflops
,
Beaverton, OR
Overall rating:
3.0 out of 5
"Torn between liking the product and it not functioning correctly. I really like the way it is laid out, the functions, the way it looks, the thinness of it, and the performance when it was working. BUT it kept freezing up, so I sent it back. Have reordered and will give it one more try. I sure hope it was just that one tablet."