Excite™ 10  Tablet (64GB)

Excite™ 10 Tablet (64GB)

MSRP: $549.99
Excite 64gb 4.00 out of 5.0 based on 1 user reviews. Average Customer Rating: 4.00 out of 5.0
Read Reviews (1)  | Write Reviews
Accessories for the Excite™ 10 Tablet (64GB)

Accessories
Covers And Cases
Docks
Power

More Excite 10 Series Tablets
10
16GB $349.99
32GB $399.99
64GB $549.99

Excite™ 10 Tablet (64GB) Customer Reviews

Killer Tablet - outstanding product

POSTED BY: , hotlanta
Overall rating: 4.0 out of 5

"This is an outstanding tablet. This tablet is so feature rich, flexible and intuitive to use, I do not know how I have done without it. It does many things with less effort than my laptop or desktop PC's. Pros: 1) It hooks up to wifi with no problems, and the range is excellent. It hooks up in a McDonalds parking lot and works flawlessly. Same in the home. 2) I use it to monitor 10 live IP cameras at a location in another city via the internet. It has no problem handling this with the proper IP cam viewer app installed. 3) The performance is excellent. I use many different apps including games, IP camera monitors, google maps, GPS maps with routing, google sky maps, stream movies over the internet as well as from lan PC's, remotely access and control other PC's over the internet using an androidVNC app, music streaming, reading e-books, creating and managing docs like Word and Excel (with proper app), and more. The tablet never has any delay running any of these apps. It has handled all of these without mis-hap or pause (delay). 4) The GPS works quickly and flawlessly. It will even work inside my house if it can just see a window. 5) The tablet has never frozen. 6) The USB and HDMI ports work perfectly. I can easily port movies over the HDMI port to a full size LCD TV. The USB, equipped with on-the-go capability, allows thumb drives, sd cards inserted in a usb holder, and portable drives to work perfectly (as long as they are FAT formatted-NTFS does not work). 7) Battery life is as advertised. It will run about 10 hrs under steady usage. I have watched 2 hour movies with only 15% battery remaining when I started the movie. I have been impressed with battery life. Cons: 1) If you insert an SD card in the full size SD slot, you will not be able to write to the SD with any program other than the supplied Toshiba file manager. ES file explorer will write to the SD, but even this program will not erase files from the SD. You have to use the Toshiba file manager. This problem is a BIG drawback to the tablet, which is otherwise perfect in every way. Because of this one issue I have only rated the tablet 4 of 5 stars. If this was fixed I would rate the Tablet 5 stars. 2) Some reviews comment about the display bleed, and it does have a slight amount at the top of screen in 2 places. However, it has never been a distraction in anything I have done on the tablet. Most of the time the bleed is not visable or noticable."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Excite Tablets
  • 7.7 Series7.7 Series
    7.7 Series
    Fits in one hand
    High-res AMOLED & scratch resistant screen
    Quad-core processor
    Micro USB & SD ports
    Powered by Android™ 4.0
    Starts at: $499.99
  • 10 Series
    10 Series
    Sleek, stylish & durable
    High-res scratch resistant screen
    Quad-core processor
    Micro USB, HDMI & full size SD ports
    Powered by Android™ 4.0
    Starts at: $349.99
  • 10 LE Series10 LE Series
    10 LE Series
    Ultra thin design
    High-res scratch resistant screen
    Dual-core processor
    Micro USB, HDMI & SD ports
    Powered by Android™ 4.0
    Starts at: $529.99
  • 10 SE Series10 SE Series
    10 SE Series
    Affordable & durable
    High-res screen
    Quad-core processor
    Micro USB & SD ports
    Powered by Android™ 4.1
    Starts at: $299.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.