x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


Excite 10 Tablets

starting at: $ Shop 10 Series

10”: Excite™ 10 Series Tablets

Excite 10 Series

3 models available Starting at $349.99 $349.99
$549.99
Excite 10 Series 4.35 out of 5.0 based on 16 user reviews.

Customer Reviews for 10 Series

If you don't have one get it

POSTED BY: , Texas
For Model: Excite 16gb
Overall rating: 5.0 out of 5

"I love this thing it is fast, the apps work great, the movies play great, the graphics are great. Well let me just put it this way I love this thing I use it everyday to chat with friends and family, play movies, write my book and more and I can not say anything bad about it at all. If I was made to go without mine now I would go insane I love it. This is my first one and I was worried I that it would take me forever how to use it, but once I got it and started playing with it it took me no time at all to figure it out."

Excellent Tablet - great flexibility

POSTED BY: , Labadie, MO
For Model: Excite 16gb
Overall rating: 5.0 out of 5

"Like the flexibility of input options, SD, USB. Have have only a few "re-boots" in almost 1 year of use. Movies, internet, email, basically all I once did from my laptop."

Most Excellent

POSTED BY: , Greensboro,NC
For Model: Excite 16gb
Overall rating: 5.0 out of 5

"First, I got the 10 for the price of the 10LE. Second, the Quad Core is fast with great graphics. The sound is fantastic for a tablet. I use iPhone ear buds. My first Ice cream Sandwich Droid, so next review will most likely tout that. Battery life is better than anything I use. File manager was real easy to use. Songs,Pics. Great Holiday gift. You'll leave the laptop for this one."

great tablet

POSTED BY: , plano, tx
For Model: Excite 32gb
Overall rating: 4.0 out of 5

"the only thing that keeps this from being a 5 star rating is the location of the recharge port"

dont buy till they update or fix

POSTED BY:
For Model: Excite 16gb
Overall rating: 1.0 out of 5

"The 4.0 isc does not work on this product and makes it run terrible. So I would recommend to stay away till they fix. You can look at their forum and see people complaining and they have done Nothing to fix it. They don't even have a answer."

Great Tablet, but not excellent.

POSTED BY: , Sacramento
For Model: Excite 16gb
Overall rating: 4.0 out of 5

"Great hardware performance except there are a lot of light bleeding at the edge of the screen. Also the battery life does not even come close to what is advertised. I would recommend if AND ONLY IF it's upgradeable to Android 4.1 (Jelly Bean)."

Great Tablet

POSTED BY: , MIami, Fla.
For Model: Excite 32gb
Overall rating: 5.0 out of 5

"I love this thing. This gadget will changes the way of computing. Everything a PC can do in a fantastic package. Ended up buying 2."

Killer Tablet - outstanding product

POSTED BY: , hotlanta
For Model: Excite 64gb
Overall rating: 4.0 out of 5

"This is an outstanding tablet. This tablet is so feature rich, flexible and intuitive to use, I do not know how I have done without it. It does many things with less effort than my laptop or desktop PC's. Pros: 1) It hooks up to wifi with no problems, and the range is excellent. It hooks up in a McDonalds parking lot and works flawlessly. Same in the home. 2) I use it to monitor 10 live IP cameras at a location in another city via the internet. It has no problem handling this with the proper IP cam viewer app installed. 3) The performance is excellent. I use many different apps including games, IP camera monitors, google maps, GPS maps with routing, google sky maps, stream movies over the internet as well as from lan PC's, remotely access and control other PC's over the internet using an androidVNC app, music streaming, reading e-books, creating and managing docs like Word and Excel (with proper app), and more. The tablet never has any delay running any of these apps. It has handled all of these without mis-hap or pause (delay). 4) The GPS works quickly and flawlessly. It will even work inside my house if it can just see a window. 5) The tablet has never frozen. 6) The USB and HDMI ports work perfectly. I can easily port movies over the HDMI port to a full size LCD TV. The USB, equipped with on-the-go capability, allows thumb drives, sd cards inserted in a usb holder, and portable drives to work perfectly (as long as they are FAT formatted-NTFS does not work). 7) Battery life is as advertised. It will run about 10 hrs under steady usage. I have watched 2 hour movies with only 15% battery remaining when I started the movie. I have been impressed with battery life. Cons: 1) If you insert an SD card in the full size SD slot, you will not be able to write to the SD with any program other than the supplied Toshiba file manager. ES file explorer will write to the SD, but even this program will not erase files from the SD. You have to use the Toshiba file manager. This problem is a BIG drawback to the tablet, which is otherwise perfect in every way. Because of this one issue I have only rated the tablet 4 of 5 stars. If this was fixed I would rate the Tablet 5 stars. 2) Some reviews comment about the display bleed, and it does have a slight amount at the top of screen in 2 places. However, it has never been a distraction in anything I have done on the tablet. Most of the time the bleed is not visable or noticable."

Awesomely Excite-ing

POSTED BY: , Mountain Home, ID
For Model: Excite 32gb
Overall rating: 5.0 out of 5

"The Excite Tablet is easy to use, fun and very efficient! I am impressed with the speed and performance of the Excite. I had a iPad 3 and although there are a few differences...the Excite still pleases me! Thanks Toshiba!"

Great Product!

POSTED BY: , Ft. Meade, MD
For Model: Excite 16gb
Overall rating: 5.0 out of 5

"I bought 2 of these, because I was impressed by the Tegra 3 hardware by Nvidia. It's very fluid over Samsung's tablet and it's not an Apple product (they will make you buy something and when you are abandoned, they say, "Just come and buy our new iPad 2!"). I like how this product comes with a GPS and is a compass; perfect for the road and not needed as a 10 inch phone."

Choose a pre-configured Excite™ 10 Tablet »

starting at:
$
Shop 10 Series

More Excite Tablets
  • 7.7 Series7.7 Series
    7.7 Series
    Fits in one hand
    High-res AMOLED & scratch resistant screen
    Quad-core processor
    Micro USB & SD ports
    Powered by Android™ 4.0
    Starts at: $499.99
  • 10 Series
    10 Series
    Sleek, stylish & durable
    High-res scratch resistant screen
    Quad-core processor
    Micro USB, HDMI & full size SD ports
    Powered by Android™ 4.0
    Starts at: $349.99
  • 10 LE Series10 LE Series
    10 LE Series
    Ultra thin design
    High-res scratch resistant screen
    Dual-core processor
    Micro USB, HDMI & SD ports
    Powered by Android™ 4.0
    Starts at: $529.99
  • 10 SE Series10 SE Series
    10 SE Series
    Affordable & durable
    High-res screen
    Quad-core processor
    Micro USB & SD ports
    Powered by Android™ 4.1
    Starts at: $349.99