POSTED BY:
Sammie
,
Alameda, CA
Overall rating:
3.0 out of 5
"I have owned two of these tablets. The micro SD slot in the first one did not work so I had to exchange it. After 4.5 months the touch screen in the second one kept freezing and yesterday I shipped it off to the repair facility. It is a shame that this product seems so unreliable because it is otherwise fun to use, efficient and a near laptop replacement."
POSTED BY:
golfnut
,
Austin, TX
Overall rating:
3.0 out of 5
"This tablet is ok for a tablet. The camera is good, the image is bright, and programs, for the most part, work fine. My biggest problem is when a program freezes up I can't do anything to get it unfrozen except leave the tablet on and let the battery run down. When the battery is completely dead the tablet turns itself off. You can then charge the battery, turn the tablet back on and use it again. I have tried everything else but nothing else works. This has happened 3 times on my tablet in the past 4 months. It needs a switch for disconnecting the battery."
POSTED BY:
nader13
,
Lebanon
Overall rating:
4.0 out of 5
"this tablet is awesome and a lot of features but am really shocked to see only 3 mp front camera :s when the dual core Thrive tablet has 5 mp why go they do such a thing"
POSTED BY:
FrankP
,
Lilburn, GA
Overall rating:
5.0 out of 5
"Bought it on sale for $250. I am amazed at all it can do. I prefer it to my laptop. I think is was excellent value for the money."
POSTED BY:
lacylee
,
Atlanta, GA
Overall rating:
5.0 out of 5
"This tablet is beautiful, and has wonderful calibration... Also, since I prefer android apps to apple apps, I would recommend this product over the iPad. Overall a great buy."
POSTED BY:
JMilo
,
Houston, TX
Overall rating:
4.0 out of 5
"Like current trends in marketing, Toshiba is now offering less product for the same money. The "new" SE while having Jellybean OS, has lower megapixel cameras and no mini HDMI slot. Less features compared to the previous generation Excite, but costs the same."
POSTED BY:
JimC
,
Houston TX
Overall rating:
5.0 out of 5
"I have bought and used all the tablets on the market. The Excite is the easiest to hold and use and has way more apps than i could ever use. I like it over the iPad 2 because i can insert a 64 gb SDCard and read my PDF's & Word Docs and change over to my other SD Cards and read the docs, listen to music and watch movies. Can't do that easily or as quickly on the iPad or other tablets!"