x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


Excite 10 SE Tablets

starting at: $ Shop 10SE Series

Excite™ 10 SE Series Tablets

Excite 10 SE Series

2 models available Starting at $349.99 $349.99
$399.99
Excite 10 SE Series 4.5 out of 5.0 based on 8 user reviews.

Customer Reviews for 10 SE Series

Biggest tablet problem

POSTED BY: , Austin, TX
For Model: Excite 16gb
Overall rating: 3.0 out of 5

"This tablet is ok for a tablet. The camera is good, the image is bright, and programs, for the most part, work fine. My biggest problem is when a program freezes up I can't do anything to get it unfrozen except leave the tablet on and let the battery run down. When the battery is completely dead the tablet turns itself off. You can then charge the battery, turn the tablet back on and use it again. I have tried everything else but nothing else works. This has happened 3 times on my tablet in the past 4 months. It needs a switch for disconnecting the battery."

wonderful

POSTED BY: , daytona beach,fl
For Model: Excite 32gb
Overall rating: 5.0 out of 5

"can't say enough wonderful things about this tablet. for the beginner like myself,its so easy to use. believe me you won't go wrong with this tablet!"

great but...

POSTED BY: , Lebanon
For Model: Excite 16gb
Overall rating: 4.0 out of 5

"this tablet is awesome and a lot of features but am really shocked to see only 3 mp front camera :s when the dual core Thrive tablet has 5 mp why go they do such a thing"

Elegant tablet that performs great

POSTED BY: , Santa Clara, CA
For Model: Excite 32gb
Overall rating: 5.0 out of 5

"The new Excite 10 SE is a no nonsense tablet running Jelly Beans version that performs very well. It is very light weight for its size. Overall good price to performance."

My First Tablet

POSTED BY: , Lilburn, GA
For Model: Excite 16gb
Overall rating: 5.0 out of 5

"Bought it on sale for $250. I am amazed at all it can do. I prefer it to my laptop. I think is was excellent value for the money."

Awesome Tablet

POSTED BY: , Atlanta, GA
For Model: Excite 16gb
Overall rating: 5.0 out of 5

"This tablet is beautiful, and has wonderful calibration... Also, since I prefer android apps to apple apps, I would recommend this product over the iPad. Overall a great buy."

Less Features on this generation

POSTED BY: , Houston, TX
For Model: Excite 16gb
Overall rating: 4.0 out of 5

"Like current trends in marketing, Toshiba is now offering less product for the same money. The "new" SE while having Jellybean OS, has lower megapixel cameras and no mini HDMI slot. Less features compared to the previous generation Excite, but costs the same."

Best Tablet Available To Date

POSTED BY: , Houston TX
For Model: Excite 16gb
Overall rating: 5.0 out of 5

"I have bought and used all the tablets on the market. The Excite is the easiest to hold and use and has way more apps than i could ever use. I like it over the iPad 2 because i can insert a 64 gb SDCard and read my PDF's & Word Docs and change over to my other SD Cards and read the docs, listen to music and watch movies. Can't do that easily or as quickly on the iPad or other tablets!"

Choose a pre-configured Excite™ 10 SE Tablet »

starting at:
$
Shop 10SE Series

More Excite Tablets
  • 7.7 Series7.7 Series
    7.7 Series
    Fits in one hand
    High-res AMOLED & scratch resistant screen
    Quad-core processor
    Micro USB & SD ports
    Powered by Android™ 4.0
    Starts at: $499.99
  • 10 Series10 Series
    10 Series
    Sleek, stylish & durable
    High-res scratch resistant screen
    Quad-core processor
    Micro USB, HDMI & full size SD ports
    Powered by Android™ 4.0
    Starts at: $349.99
  • 10 LE Series10 LE Series
    10 LE Series
    Ultra thin design
    High-res scratch resistant screen
    Dual-core processor
    Micro USB, HDMI & SD ports
    Powered by Android™ 4.0
    Starts at: $529.99
  • 10 SE Series
    10 SE Series
    Affordable & durable
    High-res screen
    Quad-core processor
    Micro USB & SD ports
    Powered by Android™ 4.1
    Starts at: $349.99