Thrive™ 10" Tablet (16GB)

Thrive™ 10" Tablet (16GB)

MSRP: $399.99
Thrive 16gb 4.44 out of 5.0 based on 93 user reviews. Average Customer Rating: 4.44 out of 5.0
Read Reviews (93) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at this similar line of laptops:
10 Series »
Accessories for the Thrive™ 10" Tablet (16GB)

Accessories
Covers And Cases
Docks
Power

Thrive™ 10" Tablet (16GB) Customer Reviews

technical problem software bluetooth defect

POSTED BY: , kuwait
Overall rating: 3.0 out of 5

"Good thrive.I own the 32 GB.but after install new android 4.0.4,the Bluetooth is visible but not connect or receive any file.even not coloured blue like other icons when it s working.do anyone help me to fix this problem.or someone know how to make a hard reset.thanks for support"

Not rootable

POSTED BY: , DC
Overall rating: 1.0 out of 5

"If I own the device I should be able to do to what I want to it. This device is not rootable AVOID at all cost."

10" Thrive Perfect device

POSTED BY: , SW Ohio
Overall rating: 5.0 out of 5

"The 10" Thrive is the perfect device. With the Full size USB and HDMI ports, removable battery. I love it. Pound for pound this device out last and out performs all other devices. I don't know why they changed it on the Excite."

Great Product!

POSTED BY: , Galveston, TX
Overall rating: 5.0 out of 5

"We bought two of these for my sons (3 & 7) for Christmas. They are the best ever! The only problem I have is that one screen got cracked and it very expensive to get it replaced or fixed. Almost the same price as we paid for the tablet. The good news is we just put a screen cover on it and it is still 100% functionable. It is so great that they can do anything and everything on their tablets. They can play games, watch movies on Netflix, get on the internet. It is great for the house and is great in the car. They battery lasts a long time and charges very quickly. I use their tablet all the time and if I purchase one for myself, I will definately get a Thrive!"

Don't do 4.0

POSTED BY: , USA
Overall rating: 3.0 out of 5

"32G 10" pre-4.0 very pleased. Installed 4.0 ... slowed system to a crawl. Taps require long touches to be recognized. 4.0 looks better but bogs things down. Ran faster with 3.x. Version 4.0.4 installed. Toshiba needs to fix this fast. Will get more stars as speed is regained."

Love it!

POSTED BY: , Massachusetts
Overall rating: 5.0 out of 5

"I bought my Thrive A100 around Christmas when I got tired of struggling with the iPad. I have not regretted the switch. It is very user-friendly and does everything I want. I even found an Epson program to connect to my printer. I use my tablet for school and internet searches. I am really glad that it works with Adobe products. That was my biggest complaint about the iPad."

Android 4

POSTED BY: , Inland Empire CA
Overall rating: 3.0 out of 5

"I have the toshiba thrive 32G 4G everything is with it the problem I having is that I heard the new android 4 system is now available for the thrives however, everytime I used the service station it says that there's no update available at this time does any body knows how to make this update Thanks"

Best Android Tablet I've found

POSTED BY: , Texas
Overall rating: 5.0 out of 5

"I've had mine since Christmas Day 2011 and I have used it everyday since. I had actually ordered Sony's Tablet S for myself, and found out that my father had bought me this, so I cancelled the order for the Sony so as to not enrage "Pa-zilla". I was skeptical at first, as I had fallen in love with the Sony's RF Universal Remote Feature, TruBlack Screen, and the whole Playstation Store integration, but I was in for a shocker with the Thrive. It has a beautiful screen, and all the useable ports have been a lifesaver. The only thing that made it better was an externally powered USB hub, which lets me use my TrackBall Mouse, External HDD, and my Printer all at once. The full HDMI port means I can do all my web browsing on my 42" TV and then switch and watch a movie from my HDD through my tablet. The only reason I still use my laptop is because the android version of Firefox still gives me headaches with flash, I can't play LOTR: Battle for Middle Earth II on Android, and I haven't come across an actual IDE for Android."

Love It!!

POSTED BY: , Tacoma WA
Overall rating: 4.0 out of 5

"I have had mine for a year plus and do not have any issues with it. I make sure to clean it up all the time and it runs great!!!"

Could be better

POSTED BY: , Chicago
Overall rating: 3.0 out of 5

"I find the processor way too slow for my needs. I surf the web, I game, and I watch tons of YouTube videos. The tablet lags when switching home screens and I don't like it. Android 4.0 is coming in the fall and that's the only thing I am looking forward to. After a year of using my thrive I can confidently say I wish I had bought some other tablet like the Samsung galaxy tab 10.1"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.