Toshiba 42TL515U  - 42" class 1080p 240Hz 3D LED TV

Toshiba 42TL515U - 42" class 1080p 240Hz 3D LED TV

MSRP: $1,099.99 Tv 42tl515u 3.93 out of 5.0 based on 13 user reviews. Average Customer Rating: 3.93 out of 5.0
Read Reviews (13)  | Write Reviews

May also be available at these dealers

Toshiba 42TL515U 42" class 3D LED TV Customer Reviews

Made and Assembled by Toshiba...

POSTED BY:
Overall rating: 5.0 out of 5

"SHOPPING TIP HERE: This is one of the few television models manufactured by Toshiba from its own factory."

3D TV

POSTED BY: , Huntington Park, Ca.
Overall rating: 3.0 out of 5

"The internet features in this TV are to poor I'm very disappointed with this features that are nothing to see or to take interest on watch all applications,because all are TV and nothing else no more channels of music, sorry Toshiba but you failed on get customer satisfaction on this mater on internet connect applications .."

Outstanding Value

POSTED BY: , Tampa Bay,Fl
Overall rating: 5.0 out of 5

"More than please with this new set. The base was shattered in transit but that was a FedEx issue and not an issue with the set. The quality to price ratio is far better than any of the other set that I compared in the weeks before deciding on this set. Yes it does take 10-15 seconds to power up but the picture is outstanding once it comes up.Customer service was easy to reach and helpful more than making up for the lacking instructions."

Great TV, needs iPhone App

POSTED BY: , USA
Overall rating: 3.0 out of 5

"This TV has a great picture in 2D and 3D. The passive glasses are so much easier to wear than active. No complaints EXCEPT the lack of iPhone app to control the TV via Wifi (like is available for most other Net TVs available)."

Needs iPhone App!!!!

POSTED BY: , US
Overall rating: 3.0 out of 5

"Great TV, but Toshiba REALLY needs to make an iPhone/Smartphone app available in the US. That's half the charm of getting a wifi TV in my opinion."

Great 3D Smart TV

POSTED BY:
Overall rating: 4.0 out of 5

"Pros: Picture/video quality, ease of setup/use. Cons: Slow response when first turned on. Built-in media center (music/photos/video) does not support NTFS file system."

Toshiba HDTV

POSTED BY: , NYC
Overall rating: 5.0 out of 5

"Bravo Toshiba!!! Exellent picture quality and amazing 3D effects!!! The only problem was the lack of information in the instruction manual however, there is a 1800 number you can call if you need help with the installation. Overall very happy with our purchase."

Great TV

POSTED BY: , Conn
Overall rating: 5.0 out of 5

"Had a Hitachi 42" Before which was a great TV But this TV is awesome! Great features and GREAT picture! Has a little wait to turn on but most computers and things with hard drives take some waiting but worth the wait!!"

Great TV

POSTED BY: , Howell MI
Overall rating: 5.0 out of 5

"We had no idea what tv to buy. I knew Toshiba made a good laptop so we deceided to look at their tv's. We found this tv and stopped looking. The quailty of the HD picture is fantastic. The only draw back is the poor sound quality. We will be getting a sound bar, which seems to be the norm for a flat screen tv."

Fantastic!

POSTED BY: , Philadelphia,Pa.
Overall rating: 5.0 out of 5

"I don't do reviews but I thought I should with this tv. The picture is perfect! I've read where folks are not happy with this tv, but I have nothing but prasies for this set. The 3D is great as well..... All have to say is great job toshiba! It's a good purchase for my money."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More TVs
  • Internet TVsInternet TVs
    Internet TVs
    Built-in Wi-Fi®
    Superior visuals
    Internet TV Apps
    Ultra thin and elegant design
    Power-efficient TVs
    Starts at: $849.99
  • 3D TVs
    3D TVs
    3D entertainment
    Stunning visuals
    Built-in Wi-Fi®
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $849.99
  • LED TVsLED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $199.99
  • LCD TVsLCD TVs
    LCD TVs
    Brilliant high-definition visuals
    Clear natural sound
    Convenient set of connectivity features
    Various screen sizes
    Starts at: $349.99
  • TV/DVD CombosTV/DVD Combos
    TV/DVD Combos
    Convenient two-in-one device
    High Definition 720p viewing
    Eco-smart design
    Wall-mountable
    Starts at: $249.99