MSRP†: $2,599.99
Average Customer Rating:

Read Reviews (4)
POSTED BY:
Don544
,
Great Lakes
Overall rating:
1.0 out of 5
"Bought this and a Blu-ray player, this shuts of and turns on screen when it feels like it, front end for netflix requires that you add movies from a computer or phone , does not allow from TV. The Blu-ray will not restart after shutdown unless unplugged and allowed to reboot from power failure, the wireless is lousy on the TV and yet is excellent on the Blu-ray (when it works at all) that is side by side. Problems persist even after new firmware/software updates. All in all sorry I bought and am going to send back."
POSTED BY:
TMC
,
Concord, OH
Overall rating:
5.0 out of 5
"I love my Toshiba 3D TV. Great price, great product, by far the best picture ever!"
POSTED BY:
Onix
,
San Francisco, CA
Overall rating:
3.0 out of 5
"The DLNA and Media Server application is next to worthless for movies. It is not clear what the format restrictions are, and even via direct input through USB, renaming avi files to mpg, mp4, etc. have continued to give "Media Playback Error". The same DLNA server on my PC served to a Sony PS3 absolutely fine, playing almost every format I sent to it, including mkv, flash, and xvid formats. I had high hopes for this TV given its internet application suite and built-in WiFi. I will leave out hope that one day through a FIRMWARE UPGRADE they will solve their playback errors. I suspect this is due poor built-in codecs that are not sufficiently robust (as another poster has noted). The 7,000,000:1 Contrast Ratio specification is highly misleading, in fact, I would go so far as to say it is erroneous and inaccurate. True blacks are far from blacks. One other minor annoyance is that there is no analog audio output to hook up to my old amplified. There is only an optical digital out. I have not tested in 3D, but even with these issues, I would give it 4 stars due to its cheap cost."
POSTED BY:
Mike
,
Cambridge, MA
Overall rating:
5.0 out of 5
"this is simply one of the best TVs currently out there. it's beautifully designed, incredibly thin and it's picture is near flawless and amazing. the 3ds are incredibly sharp and life like. standard definition picture is not as good as the others I have seen but you don't purchase a TV like this to watch SD. great sound from such a thin TV as well. the only problem I have so far with it it's inability to stay connected with the wi-fi network and it's high glossy screen which reflects any light which can ruin your viewing experience. also the stand can be a little wobbly too. overall I'm highly satisfied with this purchase."