Toshiba 40E210U - 40" class 1080p 60Hz LCD TV

Toshiba 40E210U - 40" class 1080p 60Hz LCD TV

MSRP: $549.99 Tv 40e210u 2.89 out of 5.0 based on 33 user reviews. Average Customer Rating: 2.89 out of 5.0
Read Reviews (33) 

This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other LCD TVs that are available:
LCD TVs »

Toshiba 40E210U 40" class LCD TV Customer Reviews

great buy

POSTED BY:
Overall rating: 5.0 out of 5

"nice picture cant complain a bit for the price"

POSTED BY: , BAHAMAS
Overall rating: 3.0 out of 5

"Video quality is great but the audio quality is too weak."

POSTED BY: , quebec,canada
Overall rating: 4.0 out of 5

"i've own a smaller toshiba lcd tv and i've loved it, when i wanted to get a bigger one, i've looked for panasonic or sony, than i saw this one, first thing i thaught is the picture is nicer than the previous ones. i bought it, the sound is not quite good but i dont use the tv speakers, all sound goes in stereo system. very nice picture!"

Sounding Off

POSTED BY: , Chicago, IL
Overall rating: 2.0 out of 5

"This is a nice TV and the sound is sufficient if you use it in a regular size room e.g a bedroom. I originally had the TV in my LR/DR area and the sound was awful but that is due to the space being extremely large. Once I moved the TV to my bedroom I have not had a problem with the sound. I am trying to figure out how to remove a favorite channel from the list. When I clicked on favorite it reads add/remove but it added the same channel again :("

back panel of tv has no idea of old school sound

POSTED BY: , chicago
Overall rating: 3.0 out of 5

"sound real bad output 4 audio stinks who made this tv"

Another Excellent Product!!

POSTED BY: , Kirkland, WA.
Overall rating: 4.0 out of 5

"I Love this TV! The only thing that would make it better would be to have analog audio output (R/L RCA) for easier integration. Also for people that don't realize that ANY FLAT PANEL TV has "poor quality" sound (due to basic design/size restraints) can easily plug the TV's audio into their home stereo equipment without having to upgrade all of their electronics ~ More options would be nice. I own several Toshiba products including the laptop I'm writing this with now and have been nothing but pleased, Good Job!! :)"

Great Picture/Terrible sound

POSTED BY: , MI
Overall rating: 4.0 out of 5

"I have had my Toshiba for about 10 days. I love the size of the screen and I am happy with the quality of the picture. (I'm not using the HDTV) My only issue is the sound. Its terrible. I invested in a sound bar and fingers cross it will do the trick."

Great Picture - Sound Quality Not so good

POSTED BY: , Greensboro, NC
Overall rating: 4.0 out of 5

"The picture quality is great but the sound quality is not as good as my 25 year old Sony it replaced."

*Very pleased!

POSTED BY:
Overall rating: 5.0 out of 5

"*Toshiba delete comments made by people who haven't yet received the product, or bothered to take it out of the box. Look up the definition of review! You can't do so based on OTHER reviews... If you like your eardrums then there is nothing wrong with this TV whatsoever. The sound isn't either of the extremes. If you fancy abusing your poor ears, and blasting music, and movies in them then no this isn't the TV for you. No decent priced TV alone is. You can't expect the absolute best if you're not willing to pay the absolute most. I love this television. The picture is great, the sound is just fine, PC resolution is beautiful, and the price is pretty good. It's a great bargain. My only gripe is no user manual. Shame on that new trend..."

What happens with the sound?

POSTED BY: , Toronto, ON
Overall rating: 3.0 out of 5

"Toshiba would rather make it mute as the sound they installed on it is a total joke."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More TVs
  • Internet TVsInternet TVs
    Internet TVs
    Built-in Wi-Fi®
    Superior visuals
    Internet TV Apps
    Ultra thin and elegant design
    Power-efficient TVs
    Starts at: $849.99
  • 3D TVs3D TVs
    3D TVs
    3D entertainment
    Stunning visuals
    Built-in Wi-Fi®
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $849.99
  • LED TVsLED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $199.99
  • LCD TVs
    LCD TVs
    Brilliant high-definition visuals
    Clear natural sound
    Convenient set of connectivity features
    Various screen sizes
    Starts at: $349.99
  • TV/DVD CombosTV/DVD Combos
    TV/DVD Combos
    Convenient two-in-one device
    High Definition 720p viewing
    Eco-smart design
    Wall-mountable
    Starts at: $249.99