POSTED BY:
Daisy
,
Junction City KS
Overall rating:
4.0 out of 5
"The sound is excellent when advanced sound is on. The picture could be clearer, perhaps it needs more tweaking. My primary complaint would be that it ships with "auto aspect" on so that the first few days I had to resize everytime I turned the set on. On page 77 of 144 in the online manuel it explains that it must be "off" to set the picture size so that it stays on "full screen" or what ever you have chosen. Otherwise, excellent quality for a small TV. We are using it as a second set in the bedroom."
POSTED BY:
Afrikain
,
GA
Overall rating:
5.0 out of 5
"I purchased this TV just to use it as PC monitor but I ended up connecting all kind of devices to it . The image quality is great and I' am enjoying it."
POSTED BY:
Bert
,
Grosse ile, Michigan
Overall rating:
1.0 out of 5
"Purchased this TV in May as a replacement and in a few months it would not hold channels and need to be reporgramed. Then in November it simply died would not even turn on. It is currently being repaired by Toshiba under warranty, but I had to pay the shipping cost"
POSTED BY:
nick nameless
,
AZ
Overall rating:
1.0 out of 5
"This 1080p TV is more like 720p when used as a computer monitor. The picture is good but not outstanding, and motion blur is a problem with fast action. But worst of all is the sound from the internal speakers which is incredibly bad -- far, far worse than that of my 26" 720p Toshiba. Frankly the product should have never been released to the public because of such horrible sound quality. The only saving grace is the availability of digital and analog audio outputs"
POSTED BY:
TechBuyer1
,
Grand Rapids, MI
Overall rating:
4.0 out of 5
"The 24L4200U LCD set is really nice. There are aple connection options, the display is good for this smaller set, it even has an analog audio output to connect to my older audio system (although the TV audio does not port out to it (it should)). The viewing angle is okay but not as bad as some others. The system does not seem to go to sleep when the video signal is off, other sets do this. The sound quality from the set is okay, kind of cheap and tinny, but acceptable for the price. I with the analog audio output actually sent the audio from the tuner to it so I could route the audio to some other speakers with more bass. Otherwise beyond these deficiencies, it is a overall good set."
POSTED BY:
Ank
,
SF
Overall rating:
5.0 out of 5
"Ok, lets see ! Let me describe this television as the set for those who really want to switch over to 22nd century . 1. Looks - Great and Stunning, with its sleek design it makes my wall look more tech-geeky. 2. As soon as you turn on this, you are welcomed with the Japanese logo 'Toshiba' and there you go gets hooked to its amazing picture quality - Crisp, Sharp, very natural. 3. The price that I paid, makes me feel like a King as compared to its specifications. 4. Very easy to set-up. Just un-pack, hook it to the power and all set. I connected this to my blu-ray, video Quality is unmatchable. 5. Loads of In and outs at the back of the LED, Guess there is an optical out too in this one, which i still need to experience. Overall a budget LED with the excellent options to connect my whole bunch of gadgets."