Toshiba 24SL410U - 24" class 1080p 60Hz LED TV

Toshiba 24SL410U - 24" class 1080p 60Hz LED TV

Tv 24sl410u 2.79 out of 5.0 based on 44 user reviews. Average Customer Rating: 2.79 out of 5.0
Read Reviews (44) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other LED TVs that are available:
LED TVs »

Toshiba 24SL410U 24" class LED TV Customer Reviews

The audio problems do not end at the speakers.

POSTED BY: , Stevenson, AL
Overall rating: 1.0 out of 5

"The audio on this television is absolutely horrendous. I knew better than to use the default T.V. speakers because every review criticizes them (It's horrible). There is a very noticeable background humming noise when using the RCA audio-out ports. Rendering them unusable. When using the optical audio out port, the volume is more than cut in half and renders any speakers unusable. There is absolutely NO way to get decent sound out of this TV. Picture is great, but this TV is horrible"

Great TV!

POSTED BY: , Canon City, CO
Overall rating: 4.0 out of 5

"What everyone is saying is true. It does have terribly tinny built in sound, it feels like an after-thought to me. Though, it does make up in the fact that it has a lot of inputs AND gives you multiple audio output options. I am currently hooked into the speakers I use on my computer, and it sounds great! If you are concerned that the price is going to be to high with some speakers to go with it... make a quick trip to your local electronics store and get a RCA to 3.5mm jack and then a 3.5mm coupler and some good computer speakers and voila, problem fixed! If you can find a set of PC speakers with an AUX input you are in even better shape. Give the TV a try... seriously. 1080p, 2 HDMI, and tons of goodness."

Check Reviews b4 Purchase

POSTED BY: , MI
Overall rating: 2.0 out of 5

"Cannot believe the thin/tinny sound from this product. I do not agree that it is "good enough for the kitchen." In today's marketplace, I would never have expected such poor quality sound - especially from a player like Toshiba. No sound check in store - so I let picture/price sell me."

Channel input doesn't work

POSTED BY:
Overall rating: 4.0 out of 5

"Sound not great as others have said but a little soundbar fixes issue. Biggest problem is I cannot key in channel numbers with the remote. When I try it just stays on the original channel. I can scroll through using the channel up & down buttons but I would much rather be able to type in channel 129 or 327 and not have to scroll through all the channels just to get to the ones i want."

POOR AUDIO

POSTED BY: , tennessee
Overall rating: 1.0 out of 5

"i absolutely HATE the sound system on this TV. Is there anything that can be done to increase the volume ?"

Buyer beware - very poor audio quality!

POSTED BY:
Overall rating: 1.0 out of 5

"This TV has just an unacceptable audio quality. They are worse than most laptop speakers. Listening to this TV , reminded me of watching a youtube video of a recorded TV. It is difficult to understand voices when they multiple people talk at the same time (like a political panel). This was my only Toshiba purchase, and based on this alone I would not recommend them at all. However their other TVs may be quality products. This one is just very sub-par quality compared to other TVs in the same price range."

Sound is OK for kitchen

POSTED BY: , seattle, wa
Overall rating: 4.0 out of 5

"This is the best deal out there for 24 inch- 1080p- LED! Picture is fantastic & can be jacked up using video controls. The sound is better with bass all the way up. If not good enough for you, just plug in some computer speakers."

sound horrible

POSTED BY: , ct
Overall rating: 2.0 out of 5

"I have tried every option and the sound is horrible. Can you help me to get the speakers that can easily be connected to this."

sound make viewing experience horrible

POSTED BY: , Tampa, FL
Overall rating: 2.0 out of 5

"In the past 35 years all of my TV's were Toshiba's, and I was very pleased with all of them. I replaced a 14 in, 25 year old Toshiba with sound that was exceptional; sound on this unit is horrible at best. Pictures on both are excellent? Don't know how Toshiba marketing could ever pass this off as acceptable sound."

Poor Sound

POSTED BY: , Gulf Breeze, FL
Overall rating: 2.0 out of 5

"Speakers need to be upgraded as sound quality is terrible! Nice picture and auto conversion with the HDMI works nicely with programs in HD."

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $179.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $399.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.