Toshiba 32L4200U - 32" class 720p 60H LED TV

Toshiba 32L4200U - 32" class 720p 60H LED TV

  • List Price:
  • $349.99
  • Instant Savings:
  • -$30.00

Total Price:

$319.99

Buy Now
Tv 32l4200u 3.00 out of 5.0 based on 3 user reviews. Average Customer Rating: 3.00 out of 5.0
Read Reviews (3)  | Write Reviews

Toshiba 32L4200U 32" class LED TV Customer Reviews

POSTED BY:
Overall rating: 3.0 out of 5

"good tv but the menu and everything seem old."

Distorted Aspect

POSTED BY: , Durham, NC
Overall rating: 1.0 out of 5

"Initially I was fairly pleased with the TV until I read the manual and realized that even though the screen (27.5 x 15.5) is almost identical to the widescreen 16 x 9 ratio, the only was to see undistorted widescreen TV is with a 1.5 inch black band at the top and the bottom and a 3.5 inch black band on the sides. For the life of me I can't understand why ANYONE would design a TV like this one. It is a total waste of both features I was looking for, which were HD and widescreen. Fortunately I am still in trial period and will be taking this one back for refund first chance I get."

AWESOME!!!!!

POSTED BY: , plantation, FL
Overall rating: 5.0 out of 5

"I went to get the Samsung that was very similar to this model. I have a few gaming systems so I wanted a awesome TV. This Toshiba looks exactly the same as the Samsung and the picture quality is the same if not better. This Toshiba was just a little cheaper than the Samsung, thankfully. I saved money plus got the quality picture for gaming and entertainment that i needed.....Its AWESOME!"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $199.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $419.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.