Toshiba 32SL400U - 32" class 720p 60Hz LED TV

Toshiba 32SL400U - 32" class 720p 60Hz LED TV

MSRP: $699.99
Tv 32sl400u 5.00 out of 5.0 based on 1 user reviews. Average Customer Rating: 5.00 out of 5.0
Read Reviews (1) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other LED TVs that are available:
LED TVs »

Toshiba 32SL400U 32" class LED TV Customer Reviews

AWESOME LED TV

POSTED BY: , Flint, MI
Overall rating: 5.0 out of 5

"I bought this after debating to buy this or a Samsung (LCD). Samsung is suppose to be market leader and was a really nice tv. I had the salesman put the two TV side by side and I think the colors were the same, maybe even better on the Toshiba. It was really hard to tell. What sold me is the Toshiba LED is so much thinner and lighter than then the Samsung LCD and the power consumption is much less on the Toshiba LED than any other LCD. I only gave it 4 stars on features because it doesn't have the wireless features or internet on it like some do, but then this one have the price or more from those that have those features. Besides.... when you hook up a PSP3 to it, nothing beats the PS3 blue ray player and all the apps you can get from Sony on there. It is an AWESOME TV. My daughter loves it a lot and so do I when I find myself in her room watching it instead of mine :D"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $179.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $399.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.