Toshiba 32SL410U - 32" class 720p 60Hz LED TV

Toshiba 32SL410U - 32" class 720p 60Hz LED TV

Tv 32sl410u 2.71 out of 5.0 based on 12 user reviews. Average Customer Rating: 2.71 out of 5.0
Read Reviews (12) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other LED TVs that are available:
LED TVs »

Toshiba 32SL410U 32" class LED TV Customer Reviews

LED tv? do not think so...it's LCD

POSTED BY:
Overall rating: 2.0 out of 5

"Toshiba site lists this as a LED tv. The usermanual that comes with the TV says its an LCD tv. LED tvs have a good viewing angle anywhere, this tv has good viewing only from the front...LCD. Now the problem... Turn of the TV and it starts buzzzing,humming, or something, Like a circuit on the board is failing. turn on the TV and the buzzing stops. So much for being a new TV, just passed 1 year so no warranty. Toshiba products were my go to for items like this, now im thinking of going elsewhere."

Avoid this TV

POSTED BY: , New York, NY
Overall rating: 1.0 out of 5

"3 weeks after purhcasing I returned it because lines appeared on the TV. 2 weeks later I returned the next 1 because the power button would work because it would get stuck and now I have to return a 3rd for the same reason."

NEEDS FEATURES

POSTED BY: , WEST PALM BEACH, FL
Overall rating: 3.0 out of 5

"CAN NOT USE THE REMOTE WITH MY SONY DVD PLAYER. CAN NOT LOCATE A MANUAL FOR THIS TV. THIS NEEDS LOTS OF IMPROVING."

TV is OK

POSTED BY: , Cheyenne, WY
Overall rating: 4.0 out of 5

"TV is OK. Can't say same for company."

Very sharp picture compared to higher priced units

POSTED BY: , Mississauga
Overall rating: 4.0 out of 5

"This TV is perfect for a bedroom or family room...excellent picture with HD cable..... we have a competitor LED tv in another room, more expensive, but kids watch movies on this one... price was very good... need better owners manual with description of features."

Manual controls

POSTED BY: , Whitby ontario canada
Overall rating: 3.0 out of 5

"The 32" tv that I have does not have on screen display to show what is happening when you want to make changes on the tv. I see the 42" has the on sceen display to know were to find and use the controls"

Annoyances, let me count them

POSTED BY: , Redondo Beach, CA
Overall rating: 1.0 out of 5

"Channels take sometimes up to 3 seconds to display and never immediately (un-like an LG I have). Also when the channel does display, an upper left corner info block (channel number and station ID) appears for about 20 seconds unless you click the remote's "ifo" three time or click the remote's "exit" one time (and as the remote's 'channel up and down' button and others needed to rid the annoying channel info aren't conveniently located on the remote, users are forced to use two hands to easily rid the annoying channel ID block in one added click each time you change the channel) and lastly, to remove a favorite channel from your list, the remote's "100" button should've been dual labeled (as that's what removes a favorite channel, assuming you drill the manual and find where it says to press the "100" for three seconds, why "3" seconds is beyond me).."

not bad

POSTED BY: , winnipeg
Overall rating: 3.0 out of 5

"picture is ok. cannot attach to stereo for better sound as output is not to my liking remote very easy to operate."

Unsatisfactory

POSTED BY: , Cross Lake Twp, ME
Overall rating: 2.0 out of 5

"Unhappy with this product. Viewing from directly in front of TV is fine. Colors wash out (not as clear or sharp) when viewing from either side, at a different angle. Could be because it;s an LED? Also, unable to find an owner's manual."

Excellent image

POSTED BY:
Overall rating: 5.0 out of 5

"Image is nice. Black is perfect."

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $199.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $419.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.