Toshiba 39L22U - 39" class 1080p 60Hz LED TV

Toshiba 39L22U - 39" class 1080p 60Hz LED TV

Tv 39l22u 4.18 out of 5.0 based on 10 user reviews. Average Customer Rating: 4.18 out of 5.0
Read Reviews (10)  | Write Reviews

Toshiba 39L22U 39" class LED TV Customer Reviews

Great Picture

POSTED BY: , Florida
Overall rating: 5.0 out of 5

"Very satisfied with the purchase. One of the nicest clearest pictures I've seen. Hook-ups are sufficient and the styling gives nice appearance. Looking at other reviews I agree that it does take a bit long to turn on, but once it does it is worth the wait. I disagree on the one comment about flimsy stand. I know I used more than one screw to mount it and it works well. My other negative is that I think the favorite channel arrangement could be easier to use and better arranged. There was also no owners manual included. Overall though a really nice TV."

Extremely flimsy stand.

POSTED BY: , Michigan
Overall rating: 2.0 out of 5

"I bought this TV over cheaper options because I've had good experiences with Toshiba products in the past. Although the TV itself is a good value, this is a negative review simply because of the stand that came with it. I can't believe Toshiba would compromise their reputation over something this basic. The stand is unusable. It is extremely thin, and attaches with only one screw. The TV sags towards the front, and actually sways side to side. Wall mounting might be OK, but don't buy this TV if you plan table top or shelf use."

TOSHIBA 39L22U

POSTED BY: , LAS VEGAS NV
Overall rating: 5.0 out of 5

"REPLACED 32" SAMSUNG(480)SAME WIDTH MUCH BETTER PICTURE SOUND IS OK,USED IN BEDROOM, VERY HAPPY AND PRICE WAS THE DEAL MAKER!!!!!!!!!!!!!!!!!!!(I ONLY BUY SAMSUNG OR TOSHIBA)AND HAVE NEVER HAD A PROBLEM,THIS WAS $100 LESS THEN THE 37" SAMSUNG

Perfect For PC Monitor

POSTED BY: , SW Florida
Overall rating: 5.0 out of 5

"This is my second Toshiba HDTV I have used as a PC Monitor. My first was a 32 inch ( 32RV530U). I compared overall picture quality with the top three brands. I even ask several of the sales people their opinion. We all agreed, the Toshiba was the best choice. Even sitting two feet away, the picture quality is superb! HD movies are Awesome to watch. I'm very pleased with this TV/Monitor."

Can't beat the Price

POSTED BY: , New York
Overall rating: 5.0 out of 5

"I'm a big gamer, and I love to watch a lot of movies. This T.V. is perfect to do so. Also, I like connecting my Laptop to it and doing my homework."

Nice TV

POSTED BY: , Apple Valley, CA
Overall rating: 4.0 out of 5

"Very nice TV but for some reason takes a while to start!"

Great TV

POSTED BY: , Henderson, NV
Overall rating: 5.0 out of 5

"For the price and what this TV is supposed to do it is great. It has a super picture, nice sound, easy set up and is light. Yes, it does take just a tad longer to come on, but it is hardly noticeable compared to other brands."

Great TV for Price

POSTED BY: , Wilmington, NC
Overall rating: 5.0 out of 5

"This television has provided great high definition from a high quality brand along with really loud sound, not necessarily the boom you want but any normal person gets surround sound for audio. Great Product, very happy."

Where's the sound?

POSTED BY: , Los Angeles
Overall rating: 1.0 out of 5

"This TV has a great picture and sound when it works. I've had the thing one month and I lost all audio and had to return the thing. Very disappointed!"

Beautiful picture and sound but slow

POSTED BY: , Atlanta, GA
Overall rating: 4.0 out of 5

"Really nice price, picture, sound. It takes too long to start up though."

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $179.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $399.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.