Toshiba 40L5200U - 40" class 1080p 120Hz LED TV

Toshiba 40L5200U - 40" class 1080p 120Hz LED TV

MSRP: $699.99
Tv 40l5200u 4.18 out of 5.0 based on 11 user reviews. Average Customer Rating: 4.18 out of 5.0
Read Reviews (11)  | Write Reviews

Toshiba 40L5200U 40" class LED TV Customer Reviews

Beautiful Picture, but:

POSTED BY: , Portland, OR
Overall rating: 4.0 out of 5

"1. I would like to have a manual 2. I would like to know how to program so closed caption comes on atomically when I turn the TV to mute."

Great gaming and movie tv

POSTED BY: , Amelia, oh
Overall rating: 5.0 out of 5

"Too many people are complaining about low picture quality but if you buy an hd tv you need hd to really appreciate it. Great for watching bluray or playing ps3 amazing picture when being used to view hd but like all hd tvs if you watch standard def tv on it it will show you all the sins of standard def."

Good Value

POSTED BY: , Chicago, IL
Overall rating: 4.0 out of 5

"Picture=Great Sound functions= good Sound Speakers= below average manual = online Picture angle not as good as my Plasma but quality from straight on at 1080p is just as good as my 1080i plasma"

No user manual

POSTED BY: , Chesterfield, MO
Overall rating: 3.0 out of 5

"A woodsman walked into a hardware store to buy his son a new axe. The salesman told him his son could do ten times the work with a chainsaw. The man bought the chainsaw and gave it to his son. A week later the man walked back into the store to return the saw. He told the salesman his son could only do a third of the work his son was previously able to do. And, his son complained it was much too heavy. The salsman looked bewildered and decided to test the saw himself. He started the saw. The man jumped back and asked "Whats that? We didn't know it had an engine". They should really include a complete users manual. Today companies seem to assume you already know everything there is to know about there products."

Great value, Great TV

POSTED BY: , Auburn, CA
Overall rating: 5.0 out of 5

"First point of business. to "cajunlady" and "marianne". An HD tv is not worth buying unless you subscribe to HD content either through cable or satellite. The picture is only as good as the signal it receives. The picture quality of this TV is outstanding. The images "jump" off the screen. My only issue is the same as another reviewer in that there was no owner's manual included with the set. It was easy enough to set up but more detail on the features of the TV would be nice."

Great TV!!

POSTED BY: , Grand Rapids MI
Overall rating: 5.0 out of 5

"Great picture, decent sound. It also looks good when sitting there unused which was something we were looking for. Super thin. Uses less energy than a LCD which was something else we were looking for. My only complaints are minimal. 1-No owners manual, only a quick set up guide. 2-No clock even though there is a time zone and daylight savings setting in the menu. 3-The green LED that lets you know the TV is on does not stay lit when the set it off, I like it to be on when the set is off so I know it is sitting there ready for me. Turn the bluray player on and the set comes on, turn the set off and the bluray shuts off, very nice. I would defiantly recommend this to a friend. The picture is so lifelike why would you ever go outside? LOL!!"

The picture blows you away

POSTED BY: , San Antonio, TX
Overall rating: 5.0 out of 5

"After connecting the Satellite cables and the power the comments from the people in the room was so positive and wonderful. The picture jumps out at you. Switched from an LCD to this LED and it was the best change up I've ever made. Also the sound is great."

Picture is not clear

POSTED BY: , Louisiana
Overall rating: 3.0 out of 5

"The picture is not real clear. Then I was told that I would have to subscribe to HD through my cable company. I am not so sure i would ever buy another Toshiba."

Toshiba Led 40" TV

POSTED BY: , Ontario, Canada
Overall rating: 3.0 out of 5

"My picture is not as clear as my very old T.V. It is blurry at times. It is also slow to change channels. My very old T.V. was a better picture."

We both said wow!

POSTED BY: , Milwaukee, WI
Overall rating: 5.0 out of 5

"My wife and I bought this as a second TV, so we were not looking for a lot of features. We surfed over to HBO and watched the last Harry Potter. We looked at each other and said WOW! We are very impressed with the definition and clarity of picture. The sound is impressive as well."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $179.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $399.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.