Toshiba 40S51U - 40" class 1080p 60 Hz LED TV

Toshiba 40S51U - 40" class 1080p 60 Hz LED TV

Tv 40s51u 3.27 out of 5.0 based on 16 user reviews. Average Customer Rating: 3.27 out of 5.0
Read Reviews (16) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other LED TVs that are available:
LED TVs »

Toshiba 40S51U 40" class LED TV Customer Reviews

Great TV product

POSTED BY: , SJ, Puerto Rico
Overall rating: 4.0 out of 5

"Find it simply great, some difficulty with the sound and the remote control is very slow turning on and channels. The problems is not the batteries, will have to call the 800 #"

Awesome TV - 5 Stars AAAAA+++++

POSTED BY: , Long Island, NY
Overall rating: 5.0 out of 5

"Excellent Picture. Love the internet connectivity and the widgets. Very versatile selection of inputs. I can connect everything from an HD DVR to an old Nintendo game system. No problem with sound that others have reported."

audio issues ?

POSTED BY: , san francisco ca
Overall rating: 4.0 out of 5

"Great TV for the money... as good as the Direct TV HD signal allows. Easy set-up... the remote is a little funky, but easy once you get use to it."

Great TV

POSTED BY: , Visalia CA
Overall rating: 5.0 out of 5

"I Just Purchased this TV Christmas Eve. I am happy! Outstanding Picture, and OK sound. I have not had internet connect yet, but expect to with help of tech line phone help. The sound beats most internal LED units from other Makes. I am very pleased!"

Bad Sound!

POSTED BY: , San Juan, PR
Overall rating: 2.0 out of 5

"Price OK. Audio, the worst thing I've ever heard."

Undecided

POSTED BY: , RSM, CA
Overall rating: 2.0 out of 5

"Still trying to get audio out to work. TV speakers are typical...that is they suck. Cannot seem to find the menu item that will allow the TV audio to connect to my powered speakers. I'll try a little longer, then return this Toshiba and get a SONY, which I have two of and they are perfect."

Outstanding TV

POSTED BY: , K.C. Mo.
Overall rating: 5.0 out of 5

"I wanted a LED LCD TV with composite & component inputs, WiFi, HDMI, USB & PC inputs. This unit had everything I wanted. I've always had a great experience with Toshiba products so at this price I had to buy it. Excellent Picture quality, after the WiFi upgrade the sound was greatly improved. Everything works as expected. EXCELLENT TV....:-)"

No issues

POSTED BY: , Sacramento, CA
Overall rating: 5.0 out of 5

"I just installed the televsion today, and after going through the various steps have it connected to my cable, DVD player and wireless network at my home. Everything works flawlessly. I've not noticed any issues with the sound quality. It's perfect. There was a software updated available which downloaded and installed easily. Unless something breaks I can't imagine how I could be any happier. I've been testing the internet connectivity (YouTube, etc) and it all works just fine. I'd recommend this unit to anyone."

Great Picture

POSTED BY: , NJ
Overall rating: 3.0 out of 5

"The Picture quality is very good. The sound needs help. Note that I had this TV since Aug. And so far I have had two firmware update's via the internet connection which did address the sound issue. It's much improved now."

Great picture bad sound

POSTED BY: , Brentwood, tn
Overall rating: 2.0 out of 5

"I have had Toshiba TVA before and loved them. Bought this one after 3 yr old LG quit on me. But the sound is tinny, could not get more bass, in fact the bass bar and treble bars on the settings do not work. There is no change in sound. Mute works. Put a piece of foam behind it to send the sound forward but will need to buy speakers for it."

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $179.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $399.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.