Toshiba 40SL412U - 40" class 1080p 60 Hz LED TV

Toshiba 40SL412U - 40" class 1080p 60 Hz LED TV

Tv 40sl412u 3.50 out of 5.0 based on 17 user reviews. Average Customer Rating: 3.50 out of 5.0
Read Reviews (17) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other LED TVs that are available:
LED TVs »

Toshiba 40SL412U 40" class LED TV Customer Reviews

A bad egg of the batch

POSTED BY:
Overall rating: 3.0 out of 5

"We bought this TV and it's only been close to 3 months. Bought it new, wasn't used. A month after, it started acting up. Menu screen would all of a sudden pop up, it would all of a sudden change to different input, and the worse, volume would all of a sudden go all the way up and we can't turn it down at all! All happened at different times and while watching just TV. Not playing a game or off a DVD player. Very disappointed but like the TV in general. We have to unplug the TV to 'reset' until it happens again. It was a definite pain."

Speakers?

POSTED BY: , Quebec - CAN
Overall rating: 4.0 out of 5

"TV is perfect. But with 2 'LAPTOP' speakers.... My rating cant be 5 stars.. Buy a bar sound to enjoy your TV.... I don't like the fact that when you 'mute' your tv , there is a SUB-TITLE automatic ( CC1 ).. You have to select SUB-TITLE to OFF each time... I like this TV anyway even if the sounds is really cheap."

can't get full screen HD

POSTED BY: , ohio
Overall rating: 3.0 out of 5

"Nice TV, really don't care how great sound is, my issue is full screen. I can get it from analog cable, vcr and dvd but not HDMI digital cable. I'd rather have full screen than super defined picture if that is the issue but there is no option. Cable service, Time Warner, says it is not their issue so I guess it is a Toshiba software problem. I'd just like a full screen option for any input, regardless of whether it impacts quality to some extent."

Great TV but poor Sound!

POSTED BY: , Charlevoix QUÉBEC - CAN.
Overall rating: 4.0 out of 5

"Before to buy this TV, i've took a look at all comments and you all had right. This is a great TV for the price but the speakers are cheap, Even in my little bed room the sound is to 100 and the sound is almost not disturbing for the rest of the house. I dont have HD signal yet here and i dont have tested the PC and the PS3 picture quality when i will connect it , i will can more apreciate the HD . So if you buy it, think to buy a sound kits too.Its the price to pay to get slim TV....( Sorry if my ENGLIH is not correct ). Eric."

Poor Sound

POSTED BY: , Rancho Santa Margarita, CA
Overall rating: 1.0 out of 5

"This was the 4th Toshiba Television that I have owned and the first one that I was so unsatisfied with that I returned. The audio is horrible. The size of the television was achieved to the detriment of the audio. The speakers are on the back of the set! There isn't any way that it will sound good unless it is hooked up to a home entertainment system."

Great Purchase

POSTED BY: , Lansing, MI
Overall rating: 5.0 out of 5

"very clear picture (as expected); sufficient input slots; zero problems with sound (despite some reviews - not at all tinny, far more than needed volume - yet to need to put it over 10, and that's with 3 young kids running around). Only minor gripe was with remote: inconvenient to flip through menus to select desired ratio or input, would prefer more intuitive buttons"

I love this TV!

POSTED BY: , ATL
Overall rating: 5.0 out of 5

"GREAT TV! I don't have a problem with sound w/ this TV! don't listen to all those people who have a problem with the sound!!!"

Great TV

POSTED BY: , St Paul,MN
Overall rating: 4.0 out of 5

"I was sceptical because of reported sound issues but we have an older REGZA and this units sound was great for for having the speakers in the rear. do not be fooled this is a great unit"

Great picture, poor sound.

POSTED BY: , New York, NY
Overall rating: 3.0 out of 5

"I read the reviews about the poor sounding speakers before I made this purchase. And they're correct but I can live with the poor sound. However I bought this mainly to replace a dead tv that mainly used for playing online games with my xbox360. I chose this set because it has an analog audio output that I can connect my xbox headset and hear the game sound. So far it's a big disappointment, I can barely hear anything from my headset because the sound volume barely was so so low that I thought the jack was defected."

My Father-In-Law Loves It

POSTED BY: , Charlottesville, VA
Overall rating: 4.0 out of 5

"Purchased this as a Christmas gift for my father in law and he was speechless. The picture quality is exceptional and with the QAM tuner is allowing him to get the HD versions of the networks on his cable system that was previously unavaible. He is a huge Steelers fan and the day he opened it was a game and was happy than I have ever seen him. A+ Toshiba"

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $199.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $419.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.