POSTED BY:
sunshine
,
toronto
Overall rating:
2.0 out of 5
"horrible product doesn't last longer then 6 months before it starts having problems."
POSTED BY:
Mbassett
,
Las Vegas, NV
Overall rating:
5.0 out of 5
"Thinnest and Clearest TV on the market, at 120Hz, its the best quality TV overall, The wifi problem that you're having might be due to un prevalant scanning, mine works like a charm! 100% recommend to anyone looking for a stylish TV with all the specs! The picture quality is fabulous for bluray/ps3 players, although the cable quality might be lower due to large screen, most cable providers have an upgrade option that makes watching cable, EXTRAORDINARY. Not to mention, my power bill went down significantly after we got rid of the plasma, this LED is the way to go!"
POSTED BY:
John
,
Marion, NC
Overall rating:
3.0 out of 5
"TV IS GREAT PRICE, PICTURE GREAT, BUT CAN'T GET WIRELESS TO WORK, AND HAVE TO USE 2 REMOTES. ANY HELP WOULD BE APPRECIATED."
POSTED BY:
D
,
Pennsylvania
Overall rating:
3.0 out of 5
"Picture very dull and dark no matter what the adjustments. Sound/speakers is/are horrendous! ( am aware that most need external speakers but samsung and panasonics i have are much more acceptable). Picture, instructions / recommendations on settings, etc. very poor compared to other manuals for new TV;s. I am comparing to a samsung LED I have and a panasonic lcd/led and the picture doesn't come close to either of those...one more expensive and the other way less expensive but with many of the same features like the 120hz refresh and 1080P. Also, everytime you switch from an hd channel to one that's not, the picture type/size you chose changes back so each time you switch back to an hd channel you have to change it again if you want to use the full screen. On the positive side, the wireless works like a dream. It could also use a backlit remote for those smaller buttons on the control. Would say to buy another brand...you can find with the same features for around the same price.... and picture and sound will be much better."
POSTED BY:
Toshiba delivers
,
Texas
Overall rating:
5.0 out of 5
"I got this beauty just yesterday and i couldnt be more happy with my purchase. The photos on the toshiba web just dont do justice to the real thing, everything from the swivel glass stand, to the 1 inch chrome frame make an exquisite design and when i turned it on i was even more amazed with the picture quality, it blowns away my old samsung series 5 40" lcd from 2010, i think is mainly because the tosh is 120hz processing and of course led backlit wich means better colour, contrast, etc. havent tried net tv, dlna or media player yet but with wi-fi built-in i think me and this beauty will enjoy sweet movie nights in the years to come thanks toshiba"