POSTED BY:
neto
Overall rating:
4.0 out of 5
"I bought this TV on 02-12-11 brand new at the store. TV is AWSOME. Evrything is fine and great. Teh picture is bright and sharp. The veolume is loud and clean. The only thing is that on 03-14-11, the TV began to turn off and on automaticly. It would turn off an don so fast. After being unpluged and pluged back in, it worked fine, but now the volume went crazy (up and down automaticly). There is no kids in the house and when the TV is not in use, it is unpluged so I belive warranty should cover that issue. On a second note, can somebody tell me why the Pandora app plays but no sound can be heard? I have tried all the volume settings and I just can't hear the music from Pandora eventhough it shows it's playing."
POSTED BY:
LD9000
,
Rhode Island
Overall rating:
5.0 out of 5
"I am amazed at how well this TV performs. I have been a plasma fan up until now. I bought this set blind based on the specs and I am in awe of how this set can be so thin and perform the way it does. Where this set shines is in the 1080p dept. Throw in a Blu-Ray disc and hang on. The picture is astounding. I did weeks of research on this TV and read some negative reviews with issues such as clouding, bleeding, and sound issues. I have not experienced any of these issues, and the set allows countless menus and tweak options to get the picture the way you want it. I cannot remember a TV that allowed a user to tweak the settings this much and the options are countless. I would have given this a 5-star rating in the performance dept, but in calibration there are a couple of color issues such as undersaturated reds and oversaturated blues, but again most of this can be corrected to a pleasing compromise. This TV is quite possibly the most underrated and undiscovered LED on the market. Outstanding value all the way around."