x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


LED HD TVs

starting at: $ Shop LED Series

32″ to 65″ class LED HD TVs

LED TVs

24 models available Starting at $219.99 $219.99
$2,099.99
LED TVs 4.18 out of 5.0 based on 83 user reviews.

Customer Reviews for LED TVs

Great gaming and movie tv

POSTED BY: , Amelia, oh
For Model: 40L5200U 40" class LED TV
Overall rating: 5.0 out of 5

"Too many people are complaining about low picture quality but if you buy an hd tv you need hd to really appreciate it. Great for watching bluray or playing ps3 amazing picture when being used to view hd but like all hd tvs if you watch standard def tv on it it will show you all the sins of standard def."

Gosh, it's pretty!

POSTED BY: , Massachusetts
For Model: 32L1350U 32" class LED TV
Overall rating: 5.0 out of 5

"Not the first HD TV I've seen, but the first one in my living room--and I'm really impressed!"

Great Picture

POSTED BY: , Florida
For Model: 39L22U 39" class LED TV
Overall rating: 5.0 out of 5

"Very satisfied with the purchase. One of the nicest clearest pictures I've seen. Hook-ups are sufficient and the styling gives nice appearance. Looking at other reviews I agree that it does take a bit long to turn on, but once it does it is worth the wait. I disagree on the one comment about flimsy stand. I know I used more than one screw to mount it and it works well. My other negative is that I think the favorite channel arrangement could be easier to use and better arranged. There was also no owners manual included. Overall though a really nice TV."

Best Tv ever

POSTED BY: , New Brunswick, Canada
For Model: 32L2200U 32" class LED TV
Overall rating: 4.0 out of 5

"Set works well but unable to Register it on-line! Toshiba does not recognize the Model # 32" LED 32L2200U Serial # C44241C44508K1"

Extremely flimsy stand.

POSTED BY: , Michigan
For Model: 39L22U 39" class LED TV
Overall rating: 2.0 out of 5

"I bought this TV over cheaper options because I've had good experiences with Toshiba products in the past. Although the TV itself is a good value, this is a negative review simply because of the stand that came with it. I can't believe Toshiba would compromise their reputation over something this basic. The stand is unusable. It is extremely thin, and attaches with only one screw. The TV sags towards the front, and actually sways side to side. Wall mounting might be OK, but don't buy this TV if you plan table top or shelf use."

Amazing tv for the price

POSTED BY: , New London, CT
For Model: 46L5200U 46" class LED TV
Overall rating: 5.0 out of 5

"I bought this TV before going back to college this year, and I'm crazy about it. The picture is absolutely incredible. Only gripes are that it can take a long time to turn on (as much as 10 seconds), and the speakers could be better (true of any tv in this price range, though). Anyway, I'd strongly recommend buying this"

Smart tv not so smart

POSTED BY: , Lubbock tx
For Model: 55L6200U 55" Class 3D LED HD TV
Overall rating: 3.0 out of 5

"I replaced a lg smart tv with this one. I was very disappointed. I do not use vudu. Redbox cheaper. Did have netflix. My lg had games, Facebook,I could download any apps and they worked. Internet worked just like a pc. I have Hulu plus which I can't use on this tv. It's 55 inches. When movies on from Netflix they are reduced to half size. No need for bigger tv if movies are smaller. My 50 lg did not do this. Wish I had kept my lg."

Great picture and fast set up

POSTED BY: , pasadena, md
For Model: 50L5200U 50" class LED TV
Overall rating: 4.0 out of 5

"AWESOME t.v but for the price I wish id had built in Wi-Fi or an Ethernet port to connect to the internet but great setting feathers and picture display, and cool extras. Easy to reset if you mess up the picture display."

TOSHIBA 39L22U

POSTED BY: , LAS VEGAS NV
For Model: 39L22U 39" class LED TV
Overall rating: 5.0 out of 5

"REPLACED 32" SAMSUNG(480)SAME WIDTH MUCH BETTER PICTURE SOUND IS OK,USED IN BEDROOM, VERY HAPPY AND PRICE WAS THE DEAL MAKER!!!!!!!!!!!!!!!!!!!(I ONLY BUY SAMSUNG OR TOSHIBA)AND HAVE NEVER HAD A PROBLEM,THIS WAS $100 LESS THEN THE 37" SAMSUNG

Great TV!!

POSTED BY:
For Model: 50L2200U 50" class LED TV
Overall rating: 5.0 out of 5

"This is the best TV I have ever had. The sound is really good and loud."

See All Toshiba LED Televisions »

starting at:
$
Shop LED Series

More TVs
  • LED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $219.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $449.99