55L7200U 55" Class 1080P 240Hz 3D LED HD TV

55L7200U 55" Class 1080P 240Hz 3D LED HD TV

MSRP: $2,099.99
Tv 55l7200u 4.00 out of 5.0 based on 5 user reviews. Average Customer Rating: 4.00 out of 5.0
Read Reviews (5)  | Write Reviews
More SmartTVs
Model: MSRP:
42L6200U $1,199.99
47L6200U $1,149.99
47L7200U $1,599.99
55L6200U $1,699.99
55L7200U $2,099.99

Toshiba 55L7200U 55" class 3D LED TV Customer Reviews

Great TV for the money

POSTED BY: , North Vancouver BC
Overall rating: 5.0 out of 5

"It has worked flawlessly since I bought it in July. Great color great sharpness One of only 2 brand that the RIHD works with my Onkyo surrond sound system. Along with the Toshiba 3D blu-ray I save alot of money by not going to the theatre. Well worth the price!"

55L7200U Nice TV for the price

POSTED BY: , Cypress, TX
Overall rating: 3.0 out of 5

"This tv looks amazing. It gives the appearance of not having a bezel when it is off, but on you can clearly see the edge. The screen is shiny with some mat finish. Reflects lights and sun from windows. The first tv had issues. Would not turn on right out of the box. Green light would flash with no video. After sitting unplugged for the night it powered on the next morning. During a football game it was accidentally powered off. Couldn't power it on... Just a green flashing light. Had to let it sit unplugged for hours before it turned on. The replacement has been working fine up until the 5th day I had it. Turned it on and flashing green.... Hasn't done it since then. Makes me wonder true quality...."

Really good product

POSTED BY: , montreal, quebec
Overall rating: 5.0 out of 5

"i bought the 55 inch 7200 smart 3d tv. It work perfect really good picture but a little edge light in the corner but it's a really good product .... the keyboard work perfectly. Love it!"

3D is good, rest of features are terrible

POSTED BY: , Manitoba, Canada
Overall rating: 2.0 out of 5

"Cons: wireless sets the wrong network settings(IP, gateway),so you have to manually go in and set the proper ones or spend time and money running an Ethernet cable across your house. The keyboard is missing a lot of the important buttons that are on the remote(menu, OK, volume, channel) The wireless keyboard only works the menu and web browser, doesn't work in Netflix, YouTube. You cannot download additional apps other then the 5 provided with the TV. The navigation arrows on the remote are surrounded with buttons making using the remote without looking at it almost impossible. The Enter key on the keyboard doesn't confirm entry, you have to press the F4 key(Blue button). The smartTV functions are lacking compared to other manufacturers(ie. LG, Samsung) Pros: 3D works well, 2D to 3D looks alright(depending on the content being watched), you can use the realD glasses from the movie theatre(if the 4 sets of glasses are not enough). The web browser works well with the keyboard. Thin bezel around screen makes the screen feel big. Colors and brightness are sharp, even when wearing 3D glasses. Conclusion: Good if you just want a 3D TV, but problems with setup and operating the other features, makes for a headache and wasting time trying to get it to work."

the best tv ever

POSTED BY: , nashville
Overall rating: 5.0 out of 5

"well its the best tv ever i love all u can do on it"

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More TVs
  • LED TVsLED TVs
    LED TVs
    3D entertainment
    Premium full HD viewing
    Smoother, crisper images
    Ultra thin and sleek design
    Power-efficient TVs
    Starts at: $199.99
  • CloudTVsCloudTVs
    CloudTVs
    Starts at: $419.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.