x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


Camileo HD Camcorders

starting at: $ Shop CAMCORDERS Series

Camileo HD Camcorders

Camcorders

7 models available Starting at $129.99 $129.99
$279.99
Camcorders 2.84 out of 5.0 based on 29 user reviews.

Customer Reviews for Camcorders

Awesome for the price & indestructable

POSTED BY: , Corning,NY
For Model: CAMILEO® BW20
Overall rating: 5.0 out of 5

"Sharp picture, ease of use, long battery life...This camera has all that and more. I'm a Middle school science teacher who uses cameras in the classroom daily. I have a BW-10 and thought there was no better camera. I was wrong! the BW-20 is a huge improvement! Slow motion & stop motion are huge improvements over the BW-10. Still waterproof (even floating in a hot tub)! This work horse has been dropped, banged, submerged and still delivers full HD video. I totally recommend it."

Great buy for the price. 4 to 5 Stars

POSTED BY: , Norcross, GA
For Model: CAMILEO® Z100
Overall rating: 5.0 out of 5

"I've used the Z100 indoors and outdoors and was pleasantly surprised by the results. As with most camcorders the screen does wash out in very bright daylight but it helped to shoot from the shade. I have a 3D TV and my blu-ray plays mp4 video files, so I am able to watch the original files full-size right away by plugging the SD card into a USB adapter. The software supplied edits 2D and 3D, useful for trimming and linking files together. It has difficulty titling in 3D -- but it's free! And yes, you CAN order a spare battery from Toshiba. In addition to in-camera charging there are third-party external chargers available, including auto adapters. Two batteries and a 16G SDHC card gives you around three hours of recording time/space, I have already recommended the Z100 to a friend - who bought it! Don't forget to order a couple of 16G SDHC (Class 10) flash cards. Overall very pleased."

HORRIBLE

POSTED BY: , Indianapolis
For Model: CAMILEO® X416
Overall rating: 1.0 out of 5

"The Camileo X416 does not keep focus and the settings are useless. This product was not given much thought, but rather it seems it was thrown together. Toshiba needs to RECALL this item."

Poorly made

POSTED BY: , Sacramento, CA
For Model: CAMILEO® X416
Overall rating: 2.0 out of 5

"This camcorder is simple to operate, but not well made. The battery is horrible, and the switches are only average. I'm not happy with this item...I would expect better from Toshiba."

Very Nice

POSTED BY: , Denver,Colorado
For Model: CAMILEO® X416
Overall rating: 4.0 out of 5

"This is a really nice camcoder, I am not having the focusing problems others talk about , so far it is taking sharp pictures with nice realistic color."

Not what I'd hoped it would be

POSTED BY: , Salt Lake City, Utah
For Model: CAMILEO® X400
Overall rating: 1.0 out of 5

"Got the camera for our anniversay and was excited to use it for the holidays. I videoed my grandson's Christmas and other events and all seemed to go well. Until I tried to download it on my laptop so that I could transfer it to DVD later. Then that's when all my trouble started. I had loaded the software - then connected the usb port cable - yet, it kept telling me no device connected even though it was clearly connected. After hours of frustration and being non-user friendly my wife read the instruction book and hit the format your sd card and lost all the video we had recorded. Add to that the fact that I visited toshiba.com almost 4 times looking for troubleshooting methods to fix my download problem and you have a good picture of why I will never buy toshiba. It shouldn't be that complicated."

Don't know what to believe

POSTED BY: , Tucson, Az
For Model: CAMILEO® X200
Overall rating: 4.0 out of 5

"Seeing all these reviews really confuse me. They are all extreme, some say they are absolutely horrible and others say that it's amazing. I got this camera with a class 10 sd card and the image quality is actually amazing at this price. Low light performance is not so great, but that is to be expected at this price range. Pictures are horrible but are you really going to be taking pictures with this camera -_-. You can just actually take a snapshot in your editing program from your video and that will make a great picture, if you are really going to focus on pictures go look at dslr's because you are in the wrong place. The only problem I had was with the auto focus. It's a bit slow sometimes (not all the times) and close ranged focus is not good sometimes (again, not all the time). I found macro mode to help with close ranged focus, and fixing up my lighting and the background always helped on focusing on my close-ranged subject. Overall it's not a horrible camera, but I do wish some features worked better. Some people are saying the image quality is bad but that's mainly because sometimes people forget to change the quality settings (1080p 30f, 720p 60f, and the low resolution for high fps) But I think some people were thrown off because of the dark blacks the camera picks up. I personally like those dark blacks and usually I color correct to make it look like that. But if you are looking for a different look it might get in your way. Overall I like this camera."

Nice user friendly 3D Camcorder

POSTED BY: , Springfield, MO USA
For Model: CAMILEO® Z100
Overall rating: 5.0 out of 5

"I've had this camcorder for about 6 months and I love it. It's compact, easy to use and it takes great stereoscopic 3D stills. Despite what another reviewer says it does have a removable battery so if you wanted to get an extra battery you could. The battery life is really good though, so you probably wouldn't need one. If your looking for your first 3D camcorder the budget friendly Z100 is hard to beat."

Some good features

POSTED BY: , CA
For Model: CAMILEO® X400
Overall rating: 2.0 out of 5

"I see many complaints about the video being blurry from the auto-focus not working properly. I have had that problem, but can usually make it work OK. The trick seems to be to turn the camera on, open the viewfinder and have the subject framed for at least 5 seconds before recording. If I try to record immediately it is blurry. The auto-focus is not too fast. It also seems to have a problem deciding what the focus point should be sometimes. After some movement it usually will figure out what the subject is and focus OK. To avoid likely disappointment, I would advise looking at other products before buying this one."

Really Terrible!

POSTED BY: , las vegas, nv
For Model: CAMILEO® X400
Overall rating: 1.0 out of 5

"All of the Camileo cameras come with an auto-focus feature that is awful. You cannot control the focus, and there's no firmware fix or anything. It goes in and out constantly and makes for ugly videos. Do not buy this camera!!!! I'm returning mine ASAP"

See all Toshiba CAMILEO® Camcorders »

starting at:
$
Shop CAMCORDERS Series

More Video & Electronics
  • CamcordersCamcorders
    Camcorders
    Record, edit and share movies
    Capture video in 1080p high definition
    Thin and lightweight design
    Output content via HDMI
    Starts at: $129.99
  • Audio for VideoAudio for Video
    Audio for Video
    Rich and Powerful 3D Sound
    Multiple Device Connectivity
    Simplicity and Convenience
    Built in Dolby® Digital Decoding
    Starts at: $159.99
  • Disc PlayersDisc Players
    Disc Players
    1080p high definition viewing experience
    Access content from other DLNA devices to share on your TV
    Wi-Fi ready models available
    Some models offer 3D capability
    Starts at: $39.99