BDX2500 Wi-Fi Ready Blu-ray Player

BDX2500 Wi-Fi Ready Blu-ray Player

MSRP: $179.99
Video-electronics bdx2500 1.94 out of 5.0 based on 28 user reviews. Average Customer Rating: 1.94 out of 5.0
Read Reviews (28) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Blu-ray Players that are available:
Blu-ray Players »
This product may be available at a local business reseller.

Find a Reseller

More Blu-ray Players
Model: MSRP:
BDK21 $79.99
BDX3300 $119.99
BDX5300 $139.99

Toshiba BDX2500 Customer Reviews

Problem Blu-Ray

POSTED BY: , Morrisville, NC
Overall rating: 2.0 out of 5

"I would not recommend this unit to anyone, mine works, but not the way it is suppose to. I have to unplug it after each use as it constantly turns off and on by itself. The HDMI port died months after I purchased."

horrible horrible

POSTED BY: , CT
Overall rating: 1.0 out of 5

"this blu-ray player is junk if you have a network that has even the smallest weakness it will find it. As a streaming device its awful it freezes if the program runs into trouble and you must unplug the box to fee it from its funk and maybe it will work again. The DVD/Blu-Ray function is OK i guess but at times it can be slow but no freezes on that part. My suggestion find a different player if disks are what you primarily what you use. If your looking for streaming ability use a stand alone media player (eg. ROKU). Skip this one folks!!!!!!!!!"

ITS A BIG HEADACE

POSTED BY: , San Antonio, TX
Overall rating: 1.0 out of 5

"It will freeze up sometimes, looses signal to tv, big delay between button pushes, have to unplug to unfreeze and start over. I expected better out of a Toshiba product. It take too much time and attention. I wouldnt buy it again."

Don't do the most basic thing

POSTED BY: , Gaithersburg, MD
Overall rating: 1.0 out of 5

"The most basic thing it should do it to power on, it won't even do that so it is totally useless. I bought the BDX2500 last year, the first few months I can unplug the power cord and restart the machine but now that won't do the trick. I have 15 years old DVD player that still work yet this Blu-ray player play perhaps total 20 times and now it totally dead."

its worth it

POSTED BY: , deer park ny
Overall rating: 4.0 out of 5

"this dvd player was well worth the investment.it quality is top notch the sound is great and i think i got my money worth.the price is very fair too."

poor working blu-ray

POSTED BY: , rhsc
Overall rating: 1.0 out of 5

"picture quality is awesome for the Blu-ray, Streaming is ok, lots of lost fidelity and video dynamics. Loda time for anything is very slow once you can finally get the unit to turn on. I am glad that Toshiba is not defined by this machine, cause if that were the case all products would be junk. This unit is glitchy , slow, and plain out a pain in the butt to use. I would not recommend this unit for anyone at any price level it is offered at."

DO NOT BUY HORRIBLE PRODUCT

POSTED BY: , Manteca
Overall rating: 1.0 out of 5

"Doesnt play have to unplug and plug it back it to turn it off and on. Works only when it wants to. I would return it if it wasnt a gift."

Horrible

POSTED BY: , Manteca
Overall rating: 1.0 out of 5

"I won this at a Christmas party and I couldnt even use it. I too have to unplug it and plug it back in to turn on or off. DO NOT BUY! I cant believe its even on the market. What a gift???? U YUCK"

Stay away from this one

POSTED BY: , Westminster
Overall rating: 2.0 out of 5

"Like most other reviews, this dvd player gets stuck and and you have to hold the power botton for a long time to response. It has been very frustrating. I bought since I have a 52" toshiba regza and wanted to keep them all the same brand. Very dissapointed with the bdx2500. Should have goe with the samsung."

No problem Blu-Ray DVD Player

POSTED BY: , Summerville, SC
Overall rating: 5.0 out of 5

"I have been truly impressed with this product and all its features. I have experienced no difficulties in the setup or operating of this product, completely the opposite of other customers."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Video & Electronics
  • CamcordersCamcorders
    Camcorders
    Record, edit and share movies
    Capture video in 1080p high definition
    Thin and lightweight design
    Output content via HDMI
    Starts at: $129.99
  • Audio for VideoAudio for Video
    Audio for Video
    Rich and Powerful 3D Sound
    Multiple Device Connectivity
    Simplicity and Convenience
    Built in Dolby® Digital Decoding
    Starts at: $159.99
  • Disc PlayersDisc Players
    Disc Players
    1080p high definition viewing experience
    Access content from other DLNA devices to share on your TV
    Wi-Fi ready models available
    Some models offer 3D capability
    Starts at: $39.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.