CAMILEO® H30 1080p HD Camcorder

CAMILEO® H30 1080p HD Camcorder

MSRP: $229.99
Video-electronics camileo-h30 3.00 out of 5.0 based on 36 user reviews. Average Customer Rating: 3.00 out of 5.0
Read Reviews (36) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other Camcorders that are available:
Camcorders »

Toshiba CAMILEO® H30 Customer Reviews

Bad Video

POSTED BY: , tx
Overall rating: 3.0 out of 5

"Can not record the video but can take a picture. there is no were to repair."

easy youtube upload... NOT!!!

POSTED BY: , Sacramento, CA
Overall rating: 3.0 out of 5

"so I got this HD Toshiba Camileo camcorder with a video upload option so I can easily upload my videos straight to youtube. the problem is they load up without sound..???? when I upload them to my laptop I can watch them with the sound no problem. they're in .avi format. if I convert them to .mov or .mp4 first and then upload them to youtube they work fine. but it takes forever!!! so if this camera has this button to load the videos up to youtube directly... why doesn't it work?? I checked and youtube supports avi format... so what's the problem???"

Won't Connect to my Computer

POSTED BY:
Overall rating: 1.0 out of 5

"I downloaded the arcsoft software and then plug the camcorder in my window 7 laptop it said driver not found what do i do OMG"

Great for video Ok for pictures

POSTED BY: , WI
Overall rating: 4.0 out of 5

"We were given this as a gift when our son was just under a month old. We have been using it to record some of his most memorable moments and it works well. We are impressed with the video quality when we hook it up to the TV. We have had no problem with volume or with transfering the clips from the card to the computer. We use Microsoft Movie Maker to edit and create and have had no problems there either. As far as still pictures go, not the best camera, but it does the trick in a pinch. Overall we really like it."

Disappointment

POSTED BY: , Ravenna,Ohio
Overall rating: 1.0 out of 5

"Out of the box I notice It didn't record from the t.v. bad deal right there it did say or didn't say anywhere on the box that I could fine. Most camcorder in America do both plus there is no software in the box two edit video on the camera will not detect any video or files ether. I think you know what I'm talking about and also The guide does not give very good detail information on the camcorder ether."

Lousy audio volume AGC

POSTED BY: , ca
Overall rating: 3.0 out of 5

"The video is pretty good and the camera is easy to use but the audio volume control is terrible. I have seen many complaints about this as an on-going Toshiba problem that they just ignore. I am able to coax just barely enough audio out of the files using Avidemux at its highest manual gain. Why does Toshiba refuse to fix this junky firmware?"

Good But could be better

POSTED BY: , Mississippi
Overall rating: 3.0 out of 5

"Its a great starter camera but its not reaching my needs anymore...it would be nice if this camera had a manual focus instead cause its trying to focus on everything but what i want....cant use it with windows movie maker and don't play as good HD as i thought it would.... i need to upgrade."

Don't waste your money

POSTED BY: , Boston
Overall rating: 1.0 out of 5

"I've had this for 3 months. It stopped working all of a sudden. I bought this for my cross country trip. THe battery didn't last very long. I had a hi 8 tape recorder that lasted 10 years."

Not bad

POSTED BY:
Overall rating: 4.0 out of 5

"Working with a limited budget, I needed a video camera to capture HD quality video for image presentation I am working on. Gave this one a try. The image quality is pretty good in reasonable light...low light it gets a bit grainy and soft. Was able to shoot some time delay shot over a 40 minute period and it turned out really nice. Using the supplied software, was able to convert the .avi to .mov format in both 16:9 and 4:3 formats...looses a bit of quality in the conversion but still very exceptable for what I need. My only gripe is that I had to return the first one I purchased because after recharging it the first time it would no longer come on when openingthe viewer or pressing the on switch...not sure what happened with that. Exchanged for new one and so far so good. The remote is a nice feature as is the time lapse capability."

Save your money! Cannot edit with this!

POSTED BY: , New Jersey
Overall rating: 1.0 out of 5

"Honestly, this is the biggest waste of money that I have ever gotten myself into. I saved for weeks to buy this camera. I get it, it works ok, i film with it, i go to edit, and guess what?! IT DOESNT WORK! This camcorder only works with the included software which is terrable because you can only put your clips in a story line and you cannot edit them. It doesnt work with adobe, pinnacle, corell, and every other software. Please dont make the same mistake I did. Dont waste your money on this camcorder."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Video & Electronics
  • Camcorders
    Camcorders
    Record, edit and share movies
    Capture video in 1080p high definition
    Thin and lightweight design
    Output content via HDMI
    Starts at: $129.99
  • Audio for VideoAudio for Video
    Audio for Video
    Rich and Powerful 3D Sound
    Multiple Device Connectivity
    Simplicity and Convenience
    Built in Dolby® Digital Decoding
    Starts at: $159.99
  • Disc PlayersDisc Players
    Disc Players
    1080p high definition viewing experience
    Access content from other DLNA devices to share on your TV
    Wi-Fi ready models available
    Some models offer 3D capability
    Starts at: $39.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.