Toshiba DR430 DVD Recorder

Toshiba DR430 DVD Recorder

  • List Price:
  • $149.99
  • Instant Savings:
  • -$30.00

Total Price:

$119.99

Buy Now
Video-electronics dr430 3.26 out of 5.0 based on 33 user reviews. Average Customer Rating: 3.26 out of 5.0
Read Reviews (33)  | Write Reviews
More DVD Players & Recorders
Model: MSRP:
SD3300 $39.99
SD4300 $44.99
SD-V296 $119.99
DR430 $119.99
DVR620 $189.99

Toshiba DR430 Customer Reviews

Loose sound after using pause key

POSTED BY: , b
Overall rating: 1.0 out of 5

"Unfortunately if you are editing out commercials as you record once you use the pause button once, the unit will no longer record sound."

DR430 Defective....TWICE

POSTED BY: , Atlanta,GA
Overall rating: 1.0 out of 5

"I've had two of these machines in the past month. Cannot get it to record any shows from my DVR. Alli get is the audio....no video. I have a nice store credit to use on this website, but honestly don't see anything on here that I would use. I hooked up both of the recorders in every way possible, but still no video, just audio...Frustrating to say the least."

Good value for the money

POSTED BY: , Sturgis, MS
Overall rating: 5.0 out of 5

"I have owned my DR430 for about a month now and have found it to be user friendly and good quality recorder for the money. I am very happy with my purchase."

Great Value!

POSTED BY: , South Central Texas
Overall rating: 5.0 out of 5

"I've owned one of these units for about 3 years now, and couldn't be happier with it. The learning curve wasn't bad and it records discs nicely. Due to the low price of this machine, it is my everyday DVD and CD player, as well. (I play the Blue Ray discs on my more costly machine.) I bought this brand because I was so pleased with my Toshiba LCD TV."

Useless as a recorder

POSTED BY: , Glendora, CA
Overall rating: 1.0 out of 5

"The unit plays commercial dvd's , but won't play back what it records. Screen goes black. Toshiba replaced the first unit, replacement does exactly the same thing. Since you can't talk to anyone at Toshiba anymore, is there anyone out there that has had any experience with this??"

Not up to par

POSTED BY: , Sun City, AZ
Overall rating: 2.0 out of 5

"Bought a new DR430 Recorder/Player. Was defective from the box. The S-Video IN would not accept video from Cable box. Would only work with a yellow Video RCA cord. The Unit has no HDMI input fo bring audio and video into the unit. Has HDMI OUT port only. It does have a HDMI OUT port to TV which seemed to work well."

Great recorder

POSTED BY: , Crossville TN
Overall rating: 5.0 out of 5

"I bought this to record some shows and got a lot more then I expected . I have had this for the last four years and if any thing should happen to it You bet I will replace it with an other Toshiba !"

Great DVD Recorder

POSTED BY: , Sacramento, CA
Overall rating: 5.0 out of 5

"I purchased my DR430 in January 2012 to replace a dead Sony DVD recorder that I had owned since 2005. I had researched all of the available DVD recorders and settled on this one. Like others have said, it's important to understand the machine lacks a tuner. I mostly use the S-video input to record a signal from either my satellite receiver or my camcorder. Image quality surpasses my old Sony, and the Toshiba doesn't seem to be nearly as finicky when it comes to disc media. So far, reliability is very good. I'm a video professional, so my standards are a little higher than the average person; I'm very pleased!"

DR430 Records UVerse from 1200 Box

POSTED BY: , Danville, CA
Overall rating: 5.0 out of 5

"My Panasonic DMR-ES20 died today with a U99 code. I could not find a Panasonic replacement unit. Found this Toshiba unit, compares nicely to the Panasonic DMR-ES20, and same price point even though years apart. Hooked up to UVerse 1200 Non-DVR box via RCA cables. Tested signal from DVR through 1200 box to DR430; perfect signal pickup. Recorded from DVR through 1200 box to DR430 with no problems. DO NOT connect this unit directly to a UVerse 1225, (or newer), DVR, the DVR will pump out a copy protection signal into the DVD Recorder. You MUST connect the DR430 to a 1200 Non-DVR secondary box elsewhere in your house and run DVR shows through the 1200 box then into the DR430 to record DVR programs. MOVIE CHANNELS ON UVERSE ARE ALWAYS COPY PROTECTED, they will NOT record... ALL lower channels, (and HD counterparts), record just fine through a 1200 box. I have no knowledge on the new AT&T Wireless boxes, though. This unit is AWESOME!!!"

Good Replacement DVD Recorder

POSTED BY: , San Antonio TX
Overall rating: 5.0 out of 5

"I Frankly don't understand why so many users had problems with this recorder. Recorders without a tuner cannot be used to record from TV but must be connected to another source (i.e. VCR). I had mine up and recording in under 20 minutes, and that included the time it took to format the disc. I use DVD+RW discs, which do not have to be finalized before playing on this machine or another player. So far, I've played back only one recording and it was fine. Of course, I have no way of knowing what the future holds, But, I am optimistic."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Video & Electronics
  • CamcordersCamcorders
    Camcorders
    Record, edit and share movies
    Capture video in 1080p high definition
    Thin and lightweight design
    Output content via HDMI
    Starts at: $129.99
  • Audio for VideoAudio for Video
    Audio for Video
    Rich and Powerful 3D Sound
    Multiple Device Connectivity
    Simplicity and Convenience
    Built in Dolby® Digital Decoding
    Starts at: $159.99
  • Disc PlayersDisc Players
    Disc Players
    1080p high definition viewing experience
    Access content from other DLNA devices to share on your TV
    Wi-Fi ready models available
    Some models offer 3D capability
    Starts at: $39.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.