Toshiba DVR670 DVD Recorder

Toshiba DVR670 DVD Recorder

MSRP: $249.99
Video-electronics dvr670 2.62 out of 5.0 based on 16 user reviews. Average Customer Rating: 2.62 out of 5.0
Read Reviews (16) 
This product is no longer available at most retail stores, online retailers, resellers, or ToshibaDirect.com.
We recommend taking a look at other DVD Players & Recorders that are available:
DVD Players & Recorders »

Toshiba DVR670 Customer Reviews

10 min no pic

POSTED BY: , Buffalo, mn
Overall rating: 3.0 out of 5

"The machine worked fine first 5 months then just latly last 2 weeks it started to send no pic or sound to the TV. The tape was still playing but no picture. I would have to push the play button to make the pic come to TV. It takes 10 minutes and no pic, always 10 minutes over and over all the way though the tape. Ive unplug the recorder to see if that would fix it no it didn't. Manual doesn't talk about this happening. I didn't see it in the manual.The tape works fine in my other players."

Worst ever

POSTED BY:
Overall rating: 1.0 out of 5

"I have gone through six of these in about 8 months. All failed--some as quickly as three days. Stay clear!"

Toshiba DVR670

POSTED BY: , NH
Overall rating: 5.0 out of 5

"This unit performs Excellent. The DVD picture quality is clear and stable. Set-up is easy. I have used other VHS/DVD units that were not too bad in picture quality but, the Toshiba DVR670 blows them away."

Learning curve

POSTED BY: , Lincoln, NE
Overall rating: 4.0 out of 5

"I wanted to convert old VHS family recordings to DVD. The instructions are a bit cumbersome but once you learn the process it is easy to make copies. The best feature is when copying a 2 hour tape it will automatically pause while you set up the next DVD for recording. Also this machine has a tuner so you can also record TV shows."

Out of Warranty

POSTED BY: , Medford, NY
Overall rating: 1.0 out of 5

"This was a Christmas gift from my daughter - last year. For the last 2 weeks it sat unplugged because the power wouldn't come on at all. Hoped it needed to be reset. Just called & it's out of warranty. Less than a year old & a top-of-the-line machine that doesn't even power up! Give me a break."

DVR670 nightmare

POSTED BY: , Tucson, Az
Overall rating: 2.0 out of 5

"I have hooked up the cables the same way for many units cannot even get the setup menu to come up put in a legal disc to watch a movie see the numbers move no video and no audio what gives"

Poor documentation; counter-intuitive operation

POSTED BY: , Scottsdale AZ
Overall rating: 1.0 out of 5

"Owner’s manual does not include instructions for the steps required to record and play back with the VCR. While I have rewound the tape several times, I could not explain to you how I accessed the rewind. I continue to mash four or more buttons in different sequences to make it happen. I have not tried to use the DVD recorder. I am frustrated and almost ready to ship this unit back to the vendor."

useless

POSTED BY: , Va
Overall rating: 2.0 out of 5

"Try this with Verizon Fios! Useless documentation. Abs. garbage"

Unreliable

POSTED BY: , St. Louis MO
Overall rating: 1.0 out of 5

"Here is the sequential list of failures I have experienced with my Toshiba DVR670KU since I put it in service Jan 2010. (1) In DVD recording mode, it recorded only the beginning and end of a program with the center missing. I stopped DVD recordings. (2) The auto clock reset function quit working. (3) When it reached the beginning of the tape in VCR rewind mode, it automatically started to play the tape forward. (4) About 90% of the time, a new channel number input was held only for about 2 to 3 seconds before it reverted back to the previous channel setting. (5) The manual clock set function also quit working, rendering programmed recording impossible."

Happy

POSTED BY: , Los Angles, CA
Overall rating: 5.0 out of 5

"This is one of the best DVD recorders still sold. The only unit I know of with an option to record in XP mode PCM for high quality audio to DVD, not to mention great video quality."

MSRP: Reseller/Retailer pricing may vary. Toshiba is not liable for pricing errors.

More Video & Electronics
  • CamcordersCamcorders
    Camcorders
    Record, edit and share movies
    Capture video in 1080p high definition
    Thin and lightweight design
    Output content via HDMI
    Starts at: $129.99
  • Audio for VideoAudio for Video
    Audio for Video
    Rich and Powerful 3D Sound
    Multiple Device Connectivity
    Simplicity and Convenience
    Built in Dolby® Digital Decoding
    Starts at: $159.99
  • Disc PlayersDisc Players
    Disc Players
    1080p high definition viewing experience
    Access content from other DLNA devices to share on your TV
    Wi-Fi ready models available
    Some models offer 3D capability
    Starts at: $39.99

Discount Shown in Shopping Cart

Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.