Total Price:
$269.99
POSTED BY:
rkoolaid
,
TX
Overall rating:
1.0 out of 5
"I've had this for about 2 months, the sub stopped working last night. I tried all the "troubleshooting" tips, even swapped cables and moved the whole thing to another room; it's dead. Setup was easy, the bar found the sub, the ARC features worked great with my TV, all was well - till the sound bar cycled on with the TV but didn't play. The signal was going from TV to sound bar, but nothing came from the sound bar. I had to cycle the sound bar off/on to get sound to start. And bluetooth works well, so long as you don't touch the bluetooth device - and it is less than 2 feet from the sound bar. Sound quality was pretty good. I really like the features, just hate the problems. This will be my last Toshiba product!"
POSTED BY:
Jimmy
,
Redmond,WA
Overall rating:
2.0 out of 5
"After a month or so a high pitch squeal has begun to sound from my sound bar, initially i thought it may be the cable box but it occurs on all HDMI inputs with my PS3 or PC connected as well. I changed cables and the only thing left to change is the soundbar. I wouldn't buy this, I've only had it for 4 months and its already playing up."
POSTED BY:
jaer56
,
westminster, vermont
Overall rating:
3.0 out of 5
"I also purchased this to bt music to and its useless for that because its cuts out constantly. It should power back up when the audio signal is received again also. If none of that is important to you then go for it."
POSTED BY:
Biff
,
Pompano Beach, FL
Overall rating:
3.0 out of 5
"I bought this soundbar for use with my Toshiba TV and I am quite happy with the sound quality. It is, however, the most annoying electronic component that I own. While it is nice that it powers down by itself when there is no audio input, it would be nice for it to power itself back up when audio input returns! This is the only audio component that I have ever seen that "forgets" its settings when you turn it off. And since my uVerse remote is incompatible with this unit, I need to keep both remotes handy to restore the audio settings."
POSTED BY:
Disappointed
,
Arizona
Overall rating:
1.0 out of 5
"Right from the start we were only able to connect using audio cables, the HDMI wouldn't work. We kept it anyway and then 2 wks later we began hearing a high pitched "whirring" sound and then there was no sound at all. Also as earlier posters said the BT cuts out frequently when using a moving iphone. We will be seeking a refund!"
POSTED BY:
LOLO
,
Grand Rapids, MI
Overall rating:
2.0 out of 5
"WE bought a 55" Toshiba TV and a sound bar since we had heard that it might be needed with that tv. The sound bar works, but it cannot work in front of the tv where you would normally put it, and we could not find any tv consoles that have a slot long enough for the 371/4 inch sound bar. We are extremely frustrated by this apparently very poor design incompatibility!"
POSTED BY:
Martin
,
Mexico
Overall rating:
1.0 out of 5
"Hi Guys! I just bought this sound bar in the US (since I'm from Mexico) and tried it for the first time with no issues. Once at home, I'm trying to start it with no succes; whenever I power it on, the display does not work, hence I cannot connect it with anything. Has anyone experienced something like this?"
POSTED BY:
Sherwin
,
Sammamish. WA
Overall rating:
4.0 out of 5
"Just started using bluetooth today. Connected to iphone and it worked just fine. Then connected via ipad Bluetooth and the bt connection cut out several times. Powered down and then powered up the sound bar, reconnected iPhone Bluetooth and it worked for a minute or so and cut out, kept retrying but it keeps cutting out. Any suggestions? Thanks"
POSTED BY:
Panda
,
Florida
Overall rating:
4.0 out of 5
"I was impressed by the power and sound this moderately priced sound bar puts out. I researched many different ones before I made my purchase. Sound is only lacking on the mid range sounds. Reviews were right about the bluetooth range. When I was about 12 feet away from the unit i had to hold my iphone/ipad still or else sound would cut out. not a huge deal but if you're looking to walk around the house and use bluetooth it probably won't work."
POSTED BY:
Ben
,
seymour, TN
Overall rating:
4.0 out of 5
"I bought this system because I wanted a Sound System that can be controlled via the TV Remote-Can't beat it. The Oper manual could use a little more info"