x

by

book details

Publisher:

Date Published:

Language:

ISBN:

Subjects:


Audio for Video

starting at: $ Shop SOUND-BARS Series

Audio for Video

Audio for Video

3 models available Starting at $159.99 $159.99
$269.99
Audio for Video 3.29 out of 5.0 based on 16 user reviews.

Customer Reviews for Audio for Video

great sound bar

POSTED BY: , tampa , FL
For Model: SBX1250 Sound Bar
Overall rating: 5.0 out of 5

"I just like the way it fits under my 40" HDTV . the sound has good quality and good base . you only have three modes to choice from , but at least I have that . some other bars I've tried the base is too loud and even scared my cats , but with this sound bar it seems more level and sounds great , good drivel also."

Incredible sound

POSTED BY: , Redwood City, CA
For Model: Mini 3D Sound Bar
Overall rating: 5.0 out of 5

"I bought this mini sound bar for portability and was not expecting something extraordinary but when started using I was really amazed, even shocked with its sound purity and quality. Even mp3 files are played incredibly. Thanks for such a great product!"

Great features, terrible product

POSTED BY: , TX
For Model: SBX4250 Sound Bar
Overall rating: 1.0 out of 5

"I've had this for about 2 months, the sub stopped working last night. I tried all the "troubleshooting" tips, even swapped cables and moved the whole thing to another room; it's dead. Setup was easy, the bar found the sub, the ARC features worked great with my TV, all was well - till the sound bar cycled on with the TV but didn't play. The signal was going from TV to sound bar, but nothing came from the sound bar. I had to cycle the sound bar off/on to get sound to start. And bluetooth works well, so long as you don't touch the bluetooth device - and it is less than 2 feet from the sound bar. Sound quality was pretty good. I really like the features, just hate the problems. This will be my last Toshiba product!"

great sound

POSTED BY: , longboat key , FL
For Model: SBX1250 Sound Bar
Overall rating: 5.0 out of 5

"I came to Toshiba and Am completely satisfied , for the value it has great sound ! it would be nice for a single adjustment for each sound level maybe , like treble ,bass etc. but regardless it does have the three mode and a 3D feature . I like my new sound bar very much . it at times sounds like in a movie theater ."

High Pitch Squeal

POSTED BY: , Redmond,WA
For Model: SBX4250 Sound Bar
Overall rating: 2.0 out of 5

"After a month or so a high pitch squeal has begun to sound from my sound bar, initially i thought it may be the cable box but it occurs on all HDMI inputs with my PS3 or PC connected as well. I changed cables and the only thing left to change is the soundbar. I wouldn't buy this, I've only had it for 4 months and its already playing up."

awsome

POSTED BY: , vancouver wa
For Model: SBX1250 Sound Bar
Overall rating: 5.0 out of 5

"just bought this soundbar a few days ago and im blown away at its power and sound toshiba nailed it right on the head 2 big thumbs up awsome job toshiba im so happy i have it"

good tv value but....

POSTED BY: , westminster, vermont
For Model: SBX4250 Sound Bar
Overall rating: 3.0 out of 5

"I also purchased this to bt music to and its useless for that because its cuts out constantly. It should power back up when the audio signal is received again also. If none of that is important to you then go for it."

Great Sound - Annoying "Features"

POSTED BY: , Pompano Beach, FL
For Model: SBX4250 Sound Bar
Overall rating: 3.0 out of 5

"I bought this soundbar for use with my Toshiba TV and I am quite happy with the sound quality. It is, however, the most annoying electronic component that I own. While it is nice that it powers down by itself when there is no audio input, it would be nice for it to power itself back up when audio input returns! This is the only audio component that I have ever seen that "forgets" its settings when you turn it off. And since my uVerse remote is incompatible with this unit, I need to keep both remotes handy to restore the audio settings."

Doesn't Last!

POSTED BY: , Arizona
For Model: SBX4250 Sound Bar
Overall rating: 1.0 out of 5

"Right from the start we were only able to connect using audio cables, the HDMI wouldn't work. We kept it anyway and then 2 wks later we began hearing a high pitched "whirring" sound and then there was no sound at all. Also as earlier posters said the BT cuts out frequently when using a moving iphone. We will be seeking a refund!"

Incompatible tv and sound bar

POSTED BY: , Grand Rapids, MI
For Model: SBX4250 Sound Bar
Overall rating: 2.0 out of 5

"WE bought a 55" Toshiba TV and a sound bar since we had heard that it might be needed with that tv. The sound bar works, but it cannot work in front of the tv where you would normally put it, and we could not find any tv consoles that have a slot long enough for the 371/4 inch sound bar. We are extremely frustrated by this apparently very poor design incompatibility!"

See all Toshiba Sound Bars »

starting at:
$
Shop SOUND-BARS Series

More Video & Electronics
  • CamcordersCamcorders
    Camcorders
    Record, edit and share movies
    Capture video in 1080p high definition
    Thin and lightweight design
    Output content via HDMI
    Starts at: $129.99
  • Audio for Video
    Audio for Video
    Rich and Powerful 3D Sound
    Multiple Device Connectivity
    Simplicity and Convenience
    Built in Dolby® Digital Decoding
    Starts at: $159.99
  • Disc PlayersDisc Players
    Disc Players
    1080p high definition viewing experience
    Access content from other DLNA devices to share on your TV
    Wi-Fi ready models available
    Some models offer 3D capability
    Starts at: $39.99